STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MATEKF405 firmware on custom STM32F405RGT6

I have planned to connect my custom flight controller to the ground station(mission planner) for that i have connect all the necessary connection usb connection also and flashed the pre compile firmware of matekf405 from here: https://firmware.ardupi...

Rizvi by Associate III
  • 2029 Views
  • 1 replies
  • 0 kudos

Resolved! Where to read length of sleep time on RTC WUT

We are using the STM32L071RB, currently have the firmware set to go to sleep (stop mode) and wake up after ~5 minutes with the RTC WUT (see section 22.4.6 and A13.3 in RM0377). This works great, however this timer isn't the only wakeup source. If the...

LWill.4 by Associate II
  • 3524 Views
  • 6 replies
  • 2 kudos