STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Test for EDATA FLASH ECC code on STM32H563

Hello All,We are looking into testing our code that access the EDATA and handle FLASH ECCC (single bit error) and ECCD (double bit error).How can we simulate those errors?Is it possible to insert single bit or double bit errors using a JTAG? It would...

L_P by Associate II
  • 4176 Views
  • 7 replies
  • 5 kudos

Resolved! Watermark in Azure ThreadX?

Greetings and thanks for reading.  FreeRTOS has a built in utility function uxTaskGetStackHighWaterMark() that reports on the amount of space unused by the stack.   You can use this function to gauge just how much of the stack is used and how close y...

flash erase fail

hello:      I use STM32H7A3VGT6 in our board, two flash regions are available in the MCU and their start address are 0x08000000 and 0x08080000, all in bank1, when I use STM32CubeProgrammer to erase more than 3 sectors from 0x08080000, it works well, ...

lbapplem by Associate II
  • 2564 Views
  • 4 replies
  • 0 kudos

Resolved! Blink example for STM32L552 Nucleo board

Hi! I am trying to run a simple blink example using the STM32L552 Nucleo board, but I can't seem to figure it out. Any help in figuring out what my problem is would be very helpful. I've tried looking at the data sheet to figure out what the SRAM-bou...

krook by Associate II
  • 4851 Views
  • 7 replies
  • 1 kudos

UART_WaitOnFlagUntilTimeout

i was debugging code HAL_uart_Receive (); sprintf(command, "AT+CMGL=\"ALL\"\r\n");//read all sms HAL_UART_Transmit(&huart1, (uint8_t *)command, strlen(command), 10); // HAL_Delay(100); HAL_UART_Receive(&huart1, RXbuffer, ...

Resolved! TLSv1.3 in STM32H563 using NetXSecure

Hi I'm trying to setup TLSv1.3 using STM32H63 Nucleo board. I followed the steps in https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/netx-duo/netx-duo-secure-tls/chapter3.md to enable TLSv1.3 in STM32CubeMX. But all I get from the Ope...

How to ENTDAA ( "Multiple implementation")

When executing RSTDAA and ENTDAA once, it succeeds, but when executed more than twice, it does not work properly. Since RSTDAA is being performed, I think there should be no problem, but is it not possible to execute it more than twice? //1st rstdaa+...

dai82s by Associate II
  • 1721 Views
  • 2 replies
  • 0 kudos

Resolved! AcousticBF (Beamforming) generates only noise.

I am trying to run AcousticBF (Beamforming library v3.1.0 from XCUBE_SMARTMIC_V2.4.0 pack) on STM32H747 development board, but on the output I get only a tone signal, and no audio hearable from Mics. - The inputs are two PDM mics, and the PDM signal ...

KBéla.1 by Associate III
  • 2230 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.