STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! The STM32 USB device library feels complicated

The structure of the stm32 usb device library feels very complex, is there any tutorial to clarify the structure?I want to implement a UVC.This is a picture I found on a wiki, but I can't make sense of it.For example, the file stm32xxx_ll_usb has no ...

Shiina_0-1731945993216.png Shiina_0-1732001345711.jpeg
Shiina by Associate III
  • 3553 Views
  • 5 replies
  • 6 kudos

Resolved! Hard Fault

Hello all , I am facing a issue of hard fault because of some reason however after analyzing issue I  suspect this could be due to  use of structure having uint64_t variable having bit fielding. I have also attached snapshot of issue which I am facin...

devendra_0-1732019755800.jpeg
devendra by Associate II
  • 1836 Views
  • 3 replies
  • 4 kudos

Resolved! LWIP issue in STM32H730VBT6

Hello,   I'm trying to bring up a simple ethernet client on a STM32H730VBT6 custom board. Looks like I have a 128KB of Flash and 560KB of RAM and my code would not fit into flash after I have enabled. I modified the linker script to to remap the text...

surendersampath_0-1732028992992.png

Resolved! Can't get UART Rx interrupt to work

I cannot get the RS232 Rx interrupt to work.I am working with the stm3210c-eval board. I know it is no longer available; but it has a version of the processor that I wish to use and Ethernet support.I am initiating the receive via:HAL_UART_Receive_IT...

vneff by Associate III
  • 3884 Views
  • 9 replies
  • 4 kudos

SPI Slave DMA with CRC

Dear ST,I facing a problem or bug in the calculation routine of your stm32f7xx_hal_spi.cExplicit in line 3117 of the function call:  SPI_DMAReceiveCplt()I using DMA SPI only the MOSI channel as RX_Only. This works as expected, when I dont activate CR...

UlfS by Associate II
  • 1432 Views
  • 1 replies
  • 1 kudos

Resolved! ETH LwIP program runs only when debugging

Hello ST Community!I have a problem and I need your help. I have searched and read most of the related articles but couldn't find a solution! I am using:Hardware: Nucleo H755 board connected directly to the computer.Software: STM32CubeMX version 6.12...

TonyRuan by Associate
  • 2583 Views
  • 3 replies
  • 2 kudos

Resolved! SPI DATA Stays High

I am using SPI to communicate between STM32H7B3I-DK (master) and Nucleo-H743ZI(Slave). My Data transmits as expected; however, after transmission the MISO and MOSI lines stay high. I have Master Keep IO State Enabled on both.I am not using HW NSS, an...

X_CUBE_MEMS1

Good morning,I rebuild all of the project/examples/DataLogTerminal contained in X-CUBE-MEMS1 and provided by ST without changing anything with the code generated by CubeMX.The build log gives me this error:Fatal error[Pe1696]: Unable to open source f...

Gb2 by Associate II
  • 1264 Views
  • 2 replies
  • 0 kudos