User Activity

Hi everyone, I'm deep into developing a project that is not only a passion but also a venture I'm financially invested in. I recently ordered a small batch of 50 PCBAs equipped with STM32L476RET6 microcontrollers from a well-known Chinese manufacture...
Hello ST Community,I'm currently facing a challenging issue with my STM32L476RET6 where I'm unable to erase a specific page in the flash memory. Despite the HAL_FLASHEx_Erase() function returning HAL_OK, indicating the erase operation was supposedly ...
Hello ST Community,I'm developing a USB CDC communication project on an STM32L476RET6 microcontroller, using STM32CubeIDE. While I can successfully receive data from a PC using PuTTY, I'm facing a challenge with transmitting data back to the PC using...
 I’m new to STM32 development so I’ve been using the CubeIDE – Device Configuration Tool to generate most of the code, and HAL calls.I’m using an stm32h747xih (Dual core M7 & M4 Discovery Board) and have being trying to get the ADCs to work. I’ve sta...