STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hard fault after lwip init

i recently made a custom board using stm32h743VIT6 and i configured lwip and freertos (before this i was using stm32f407vgt6 it is perfectly working and the circuit is same for this MCUs) now when i start the program it keeps having hardfault i tried...

Saeedn823 by Associate II
  • 2995 Views
  • 3 replies
  • 0 kudos

Reset state slave timer

Chip: STM32H747I have setup a master timer.    sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;And two slave timers each with    sSlaveConfig.SlaveMode = TIM_SLAVEMODE_COMBINED_...

Resolved! Problem writing string to emulated Eeprom

Can anyone explain to me what is wrong in my code?Microcontroller: STM32C031K6T6I'm trying to make an interface so that the user can change the name of their environment in real time, my idea and what I tried to write is something that holds the prev...

Problem with SPI and ADXL345

 Hi, I’m having trouble reading measurements from the ADXL345 using SPI. I’ve attached a picture from the debugger that shows a view of the variables. The SPI is configured as master full duplex, and I’ve included a screenshot showing the SPI configu...

FilipF303RE_0-1731342474048.png FilipF303RE_1-1731342489083.png