STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HardFault UDP Client

Hi Community, I am using the Nucleo-H723ZG board for data receiving from the camera by utilizing the spi and processing the data then transforming the data through UDP to another program. The program can run for several hours without problem. But the...

LEAMtw by Associate
  • 4570 Views
  • 8 replies
  • 12 kudos

Resolved! STM32U5G9J-DK1 SPI

Hello, I'm using a STM32U5GJ-DK1 with the same SPI setup, I can measure the SCK output on SPI2, but I can't do it on SPI3.   *This post has been translated from Chinese to comply with the ST Community guidelines.    

shenghung_1-1734056254917.png shenghung_0-1734055164426.png

Implementing FRS on G474

Dear ST Community        I recently purchased two sets of Nucleo-DRP1M1+NucleoG474, and now I want to implement FRS functionality on these two boards. Currently, I have set one of the default power roles to Source, enabled FRS_TX, and the other to Si...

AgoDream_0-1733801876086.png AgoDream_0-1733813519613.png
AgoDream by Associate II
  • 2491 Views
  • 6 replies
  • 1 kudos

Resolved! ['F446 documentation] SPDIF-Rx - sync_done

Posted on January 16, 2018 at 15:48In RM0390 rev.3, in Figure 347. SPDIFRX States, sync_done internal signal is mentioned (and nowhere else). Isn't it the same as SPDIFRX_SR.SYNCD, at least from the programmer's point of view? If so, please replace ...

Resolved! USBX - Composite USB device - CDC ACM and MSC

I'm trying to develop an application for the STM32H750 using USBX to implement two classes on the same USB device: CDC ACM and MSC. I've managed to get each one working individually, but I'm having trouble combining them. When I connect it to a PC, n...