cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I download the external loader source code of W25Q128 Nor Flash?

lucky_jeck
Associate

I found that the external loader of "STM32CubeProgrammer" includes "W25Q128JVEIQ_STM32F746G-DISCO.stldr" and "W25Q128JVEIQ_STM32F7508-DK.stldr", but please tell me where I can download the source code of these two external loaders? Because I want to modify it according to the pins of the STM32 development board and add it to my project.

W25Q128 external loader.png

 

 

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

I'm not sure ST has published their source for these. Other examples can be found on Github.

What STM32 family are you using,and what are your QSPI pin assignments?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
STea
ST Employee

Hello @lucky_jeck ,

You can refer to this github repository contains the Flashloaders source code of external memories embedded in STM32F7 HW boards.

BR

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

These don't include the Winbond models on some of the DK

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks, while there is no ready-made source code to modify, I will use MX25L512G as a reference to design my code