User Activity

I have an application using the XL function, it works fine, no issues.Now I need to read the gyroscope output data.After I finish configuring the registers:CTRL9_XL 01INT1_CTRL 03INT2_CTRL 06CTRL1_XL 30CTRL2_G 32CTRL3_C 04CTRL6_C 80CTRL8_XL 00MD1_CFG...
I am using the STM32U575xx and found stackoverflow questions regarding the DWT->CYCLCNT.c - STM32 - How to enable DWT Cycle counter - Stack Overflow I tested this and it works fine, but I'd like to have documentation aside from the header file.I'd li...
I am trying to make a sleep function that accepts a uint16_t argumentin microsecond.I wanted to use DWT->CYCCNT, but it seems the counter remains frozen.Obviously, I read the DWT_CTRL_CYCCNTENA_Pos from ->CTRL and the bit is set, therefore enabled.I ...
I noticed the CYCCNT register is accessible from multiple header files.That register is defined as part of the DWT_Type structure.That structure definition is repeated in many header files:core_armv8mbl.h, core_armv8mml.h, core_armv81mml.h, core_cm3....
Kudos given to