STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 FATFS with SPI FLASH

I am trying to interface a SPI flash from Winbond (W25Q64JV) with FATFSI have no previous experience with FATFS.I initialize FATFS in CubeMX with the option "used-defined" and modified the MAXIMUM and MINIMUM Sector Size to 4096, as it is the smalles...

mbedtls vs wolfssl

Hello!I need to set up an STM32H745 to make an HTTPS request. In the last few weeks, I have configured LWIP using this example (https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308) and se...

RafaelS by Associate III
  • 3680 Views
  • 4 replies
  • 2 kudos

Resolved! Get external I2C3 working on Sensor Tile.Box Pro

I have a Sensor Tile.Box pro and I want to communicate using I2C to an external peripheral using the PG7 and PG8 pins, which are the I2C3 SCL and SDA pins. However I am unable to get as much as basic GPIO working on those two pins, let alone I2C.I ha...

Mantis by Associate
  • 1397 Views
  • 2 replies
  • 0 kudos

Resolved! Question about pUserData field on HAL

I am developing in C++ on a STM32U5, with HAL and was trying to figure how to embed interrupt handling in a class.So I've questioned ChatGPT and DeepSeek for a solution and both gave an answer using pUserData field for storing object reference.pUserD...

dimercur by Associate II
  • 3515 Views
  • 10 replies
  • 6 kudos

Resolved! STM32G030F6 MCU : Shutdown mode

Hi Experts,We are building a battery based product based STM32G030F6 MCU. We are using Arduino environment as we need multiple Arduino libraries for the project.Well our software is working fine, however we are facing issue with the current consumpti...

gailu96 by Associate II
  • 4338 Views
  • 11 replies
  • 1 kudos

STM32 Canbus Multiple Device Weird İssue

I am developing a project with STM32 using the STM32G473CET6 chip and working on a CAN bus system. In this project, the STM32 sends messages to the bus, processes the received messages, and responds accordingly. For example, the message 10170001 quer...

MKT12 by Associate II
  • 2059 Views
  • 5 replies
  • 1 kudos