STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32h743 HAL PClock1 Calculation

Disclaimer: I don't normally use HAL, but I was trying to learn more about USB hosting so I decided to try out the demonstration application STM32Cube_FW_H7_V1.12.0 STM32H743I-EVAL USB_Host/CDC_StandaloneAs I don't have that board, I tried to hook up...

Danish1 by Lead III
  • 3719 Views
  • 6 replies
  • 3 kudos

Resolved! Programatically (hardware) reset of STM32

Hello,program that is used to flash STM32H753VI processor (powered over USB) asks to disconnect and then connect again of USB connection to start with flashing. I found also a possibility to start with flashing without reconnecting USB, and that is w...

d3jck29 by Associate
  • 3683 Views
  • 3 replies
  • 6 kudos

STM32-H7 driver for LAN8670 external phy

Hi, I'm working on project, and as a part of it I need to establish an Ethernet connection between the 2 devices.    The device is powered by STM32H7 MCU which is connected to Microchip LAN8670 PHY (10BaseT-1s). On the other side there is or another ...

vano4411 by Associate II
  • 9347 Views
  • 7 replies
  • 0 kudos

STM32H7 SDMMC IDMA + MDMA

Hi everybody! I have searched almost half of the Internet and couldn't find any working example of these kind of technology combination: STM32H7 SDMMC IDMA + MDMA. I must say that without MDMA, everything works good (I'm aware of cache problems). But...

Zed by Associate III
  • 1956 Views
  • 1 replies
  • 1 kudos

WWDG: Getting started

Hello there,I am new to STM32 MCUs and been experimenting with different examples. I have below questions regarding WWDG.1. If you look commented section at line# 101 below. I understand the role of counter and window value but wondering where values...

Sam4 by Associate II
  • 2045 Views
  • 3 replies
  • 0 kudos

TCP communication with NetX Duo on STM32H563

I've been trying to set up TCP communication with NetX Duo on an STM32H563 now for several days with little success. I can receive one packet, but every packet sent after fails. I've gotten UDP, ICMP, DHCP, etc. to work fine, but TCP for some reason ...

brazien by Associate
  • 1028 Views
  • 1 replies
  • 0 kudos