Skip to main content
Associate II
February 12, 2025
Question

WWDG: Getting started

  • February 12, 2025
  • 2 replies
  • 875 views

Hello there,

I am new to STM32 MCUs and been experimenting with different examples. I have below questions regarding WWDG.

1. If you look commented section at line# 101 below. I understand the role of counter and window value but wondering where values 4096 and 64 are coming from?

/**
 ******************************************************************************
 * @file WWDG/WWDG_Example/Src/main.c
 * @author MCD Application Team
 * @brief This sample code shows how to use the STM32F769xx WWDG HAL API
 * to update at regular period the WWDG counter and how to simulate
 * a software fault generating an MCU WWDG reset on expiry of a
 * programmed time period.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2016 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */

/* Includes ------------------------------------------------------------------*/
#include "main.h"

/** @addtogroup STM32F7xx_HAL_Examples
 * @{
 */

/** @addtogroup WWDG_Example
 * @{
 */

/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
/* WWDG handler declaration */
static WWDG_HandleTypeDef WwdgHandle;

/* Private function prototypes -----------------------------------------------*/
static void MPU_Config(void);
static void SystemClock_Config(void);
static void Error_Handler(void);
static void CPU_CACHE_Enable(void);
/* Private functions ---------------------------------------------------------*/

/**
 * @brief Main program
 * @PAram None
 * @retval None
 */
int main(void)
{
 /* Configure the MPU attributes */
 MPU_Config();

 /* Enable the CPU Cache */
 CPU_CACHE_Enable();

 /* STM32F7xx HAL library initialization:
 - Configure the Flash prefetch
 - Systick timer is configured by default as source of time base, but user
 can eventually implement his proper time base source (a general purpose
 timer for example or other time source), keeping in mind that Time base
 duration should be kept 1ms since PPP_TIMEOUT_VALUEs are defined and
 handled in milliseconds basis.
 - Set NVIC Group Priority to 4
 - Low Level Initialization
 */
 HAL_Init();

 /* Configure the system clock to 216 MHz */
 SystemClock_Config();

 /* Configure LED1, LED2, LED3 */
 BSP_LED_Init(LED1);
 BSP_LED_Init(LED2);
 BSP_LED_Init(LED3);

 /* Configure User push-button */
 BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);
 //BSP_LED_On(LED1);
 /*##-1- Check if the system has resumed from WWDG reset ####################*/
 if (__HAL_RCC_GET_FLAG(RCC_FLAG_WWDGRST) != RESET)
 {
 /* WWDGRST flag set: Turn LED1 on */
 BSP_LED_On(LED1);
	 //BSP_LED_Off(LED1);

 /* Clear reset flags */
 __HAL_RCC_CLEAR_RESET_FLAGS();
 }
 else
 {
 /* WWDGRST flag is not set: Turn LED1 off */
 //BSP_LED_Off(LED1);
	 //BSP_LED_On(LED1);
 }


 /*##-2- Configure the WWDG peripheral ######################################*/
 /* WWDG clock counter = (PCLK1 (216MHz)/4096)/8) = 6592 Hz (~158 us)
 WWDG Window value = 120 means that the WWDG counter should be refreshed only
 when the counter is below 120 (and greater than 64/0x40) otherwise a reset will
 be generated.
 WWDG Counter value = 127, WWDG timeout = ~158 us * 64 = 11 ms */
 WwdgHandle.Instance = WWDG;

 WwdgHandle.Init.Prescaler = WWDG_PRESCALER_8;
 WwdgHandle.Init.Window = 120;
 WwdgHandle.Init.Counter = 127;

 if (HAL_WWDG_Init(&WwdgHandle) != HAL_OK)
 {
 /* Initialization Error */
 Error_Handler();
 }

 /* Infinite loop */
 while (1)
 {
 /* Toggle LED2 */
 //BSP_LED_Toggle(LED2);
 /* Insert 20 ms delay */
	BSP_LED_Off(LED1);
 HAL_Delay(20);

 /* Refresh WWDG: update counter value to 127, the refresh window is:
 between 1 ms (~158 * (127-120)) and 11 ms (~158 * 64) */

 if (HAL_WWDG_Refresh(&WwdgHandle) != HAL_OK)
 {
 Error_Handler();
 }
 }
}

 

2. There supposed to be a interrupt happening after pressing user push-button (PC.13), that should tie to EXT1 line but if you look below the interrupt handler is other than EXT1, does it mean I have create a interrupt handler for EXT1?

/******************************************************************************/
/* STM32F7xx Peripherals Interrupt Handlers */
/* Add here the Interrupt Handler for the used peripheral(s) (PPP), for the */
/* available peripheral interrupt handler's name please refer to the startup */
/* file (startup_stm32f7xx.s). */
/******************************************************************************/

/**
 * @brief This function handles External line 15_10 interrupt request.
 * @PAram None
 * @retval None
 */
void EXTI15_10_IRQHandler(void)
{
 /* As the following address is invalid (not mapped), a Hardfault exception
 will be generated with an infinite loop and when the WWDG counter falls to 63
 the WWDG reset occurs */
 *(__IO uint32_t *) 0xA0003000 = 0xFF;
}

 

3. I am looking into stm32f7xx_hal_wwdg.c file for the interrupt handler callback. I can see there is a callback " HAL_WWDG_EarlyWakeupCallback(hwwdg);" wondering if this is the callback for EXT1, to me it doesn't seem like it is. Could you explain me the how to setup IRQ handler that takes care of interrupt EXT1 which is being generated by pressing user button.

/**
 * @brief Handle WWDG interrupt request.
 * @note The Early Wakeup Interrupt (EWI) can be used if specific safety operations
 * or data logging must be performed before the actual reset is generated.
 * The EWI interrupt is enabled by calling HAL_WWDG_Init function with
 * EWIMode set to WWDG_EWI_ENABLE.
 * When the downcounter reaches the value 0x40, and EWI interrupt is
 * generated and the corresponding Interrupt Service Routine (ISR) can
 * be used to trigger specific actions (such as communications or data
 * logging), before resetting the device.
 * @PAram hwwdg pointer to a WWDG_HandleTypeDef structure that contains
 * the configuration information for the specified WWDG module.
 * @retval None
 */
void HAL_WWDG_IRQHandler(WWDG_HandleTypeDef *hwwdg)
{
 /* Check if Early Wakeup Interrupt is enable */
 if (__HAL_WWDG_GET_IT_SOURCE(hwwdg, WWDG_IT_EWI) != RESET)
 {
 /* Check if WWDG Early Wakeup Interrupt occurred */
 if (__HAL_WWDG_GET_FLAG(hwwdg, WWDG_FLAG_EWIF) != RESET)
 {
 /* Clear the WWDG Early Wakeup flag */
 __HAL_WWDG_CLEAR_FLAG(hwwdg, WWDG_FLAG_EWIF);

#if (USE_HAL_WWDG_REGISTER_CALLBACKS == 1)
 /* Early Wakeup registered callback */
 hwwdg->EwiCallback(hwwdg);
#else
 /* Early Wakeup callback */
 HAL_WWDG_EarlyWakeupCallback(hwwdg);
#endif /* USE_HAL_WWDG_REGISTER_CALLBACKS */
 }
 }
}


/**
 * @brief WWDG Early Wakeup callback.
 * @PAram hwwdg pointer to a WWDG_HandleTypeDef structure that contains
 * the configuration information for the specified WWDG module.
 * @retval None
 */
__weak void HAL_WWDG_EarlyWakeupCallback(WWDG_HandleTypeDef *hwwdg)
{
 /* Prevent unused argument(s) compilation warning */
 UNUSED(hwwdg);

 /* NOTE: This function should not be modified, when the callback is needed,
 the HAL_WWDG_EarlyWakeupCallback could be implemented in the user file
 */
}

Thanks,

 

 

 

2 replies

ST Employee
February 12, 2025

Hello @Sam4

"4096" is used to calculate the WWDG clock counter, here is the formula:

SarraS_0-1739376976439.png

"64" is used to calculate the timeout using this formula: 

SarraS_1-1739377041304.png

WWDG timeout= 158ms x (127-64) =11ms 

Regarding the interrupt handler: The interrupt handler EXTI15_10_IRQHandler handles external interrupts for lines 15 to 10, the user push-button (PC13) is connected to EXTI line 13, which falls within this range.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Sam4Author
Associate II
February 12, 2025

Hello @Sarra.S 

thanks for your quick response. regarding the 64 (window value) in the example window value is 127 (not 64) but the comment still says that the refresh time should be between 1 ms to 11 ms.

/* Refresh WWDG: update counter value to 127, the refresh window is:

between 1 ms (~158 * (127-120)) and 11 ms (~158 * 64) */

 

Also, so in the example below function is not being used? Button press is directly calling the

the "void EXTI15_10_IRQHander(void)" ?

 

void HAL_WWDG_IRQHandler(WWDG_HandleTypeDef *hwwdg)
{
 /* Check if Early Wakeup Interrupt is enable */
 if (__HAL_WWDG_GET_IT_SOURCE(hwwdg, WWDG_IT_EWI) != RESET)
 {
 /* Check if WWDG Early Wakeup Interrupt occurred */
 if (__HAL_WWDG_GET_FLAG(hwwdg, WWDG_FLAG_EWIF) != RESET)
 {
 /* Clear the WWDG Early Wakeup flag */
 __HAL_WWDG_CLEAR_FLAG(hwwdg, WWDG_FLAG_EWIF);

#if (USE_HAL_WWDG_REGISTER_CALLBACKS == 1)
 /* Early Wakeup registered callback */
 hwwdg->EwiCallback(hwwdg);
#else
 /* Early Wakeup callback */
 HAL_WWDG_EarlyWakeupCallback(hwwdg);
#endif /* USE_HAL_WWDG_REGISTER_CALLBACKS */
 }
 }
}

 

ST Employee
February 13, 2025

Hello @Sam4

The HAL_WWDG_IRQHandler function is not used for handling the button press interrupt. The button press interrupt is handled by the EXTI15_10_IRQHandler function.

The HAL_WWDG_IRQHandler function handles the WWDG interrupt request, specifically the Early Wakeup Interrupt (EWI) -you can check the HAL drivers code- 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.