User Activity

I have a system that I am migrating from a part with more RAM to the STM32H733.  I already have external FLASH set up and operating well but the amount of RAM available for heap is anemic for future growth.The external flash is running on the OCTOSPI...
We are migrating a project from H750 to H733 and I have run into an issue with our custom bootloader.We have our own External Loader, Bootloader and Application.  Works fine on 750, but I have had to remake the projects for a move to the H733 micro.W...
I'm migrating source that has run for quite a while successfully on H755 to a new project so we can swap to the H733 micro for the increased memory security features.The project is not currently using the external OCTOSPI, building a reduced version ...
We have a project that was working with a demo board with a different micro than our final project uses. We imported into CubeIDE an ioc generated by CubeMX by our hardware engineer. We did a bit of work on the project to include source from a vari...
Kudos from
Kudos given to