STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LwIP with Threadx

From my research, I've read that LwIP is written with FreeRTOS, but can be altered to support any OS. Since ST has made an effort to support/encourage LwIP and ThreadX, are there any resources/examples that we can reference?I am doing my evaluation w...

Resolved! Read GnuPG card with STM32

Hello.I have  to develop a project with Riverdi STM embedded display (that uses STM32H757). In this project I have to read the USER NAME and the SERIAL NUMBER of GnuPG smart card. I started from AN4800 that is for GSM File system Smart Card but I don...

Change uart settings and pinout runtime

Hi!I'm working with a STM32C071 and I would like to change uart1 pinout and settings runtime: I've defined USART1 (in the .ioc file) as PB2 (RX) and PC14 (TX). After boot, I would like to change the USART1 pinout as PB6 (TX) and PB7 (RX). So I've wri...

BRonc.1 by Associate III
  • 2378 Views
  • 5 replies
  • 4 kudos

gnss libary includded in X-CUBE-GNSS1 libary

i want to report a bug entered in the GNSS libary. in the LibNMEA in the file NMEA_parser.cin line 679:        if (strcmp((char *)app[0], "$GPGST") == 0 || strcmp((char *)app[0], "$GNGST"))missing the == 0 part.and in line 734        if (strcmp((char...

mfried by Associate
  • 833 Views
  • 1 replies
  • 1 kudos

Resolved! Netx / ThreadX / Compiler issue - BUG?

Hello,I started a blank project for the STM32H743 with AzRtos, ThreadX, NetXDuo..  There is something weird with the compiler and linker, or I don't understand how to setup the project...The project compiles and runs, but the memory mapping seems to ...

mattcrc_0-1739648704670.png mattcrc_1-1739648859308.png mattcrc_2-1739649146199.png mattcrc_3-1739649363435.png
matt-crc by Senior III
  • 4163 Views
  • 7 replies
  • 1 kudos