User Activity

Hello,With ST Microelectronics advising to move away from ThreadX and back to FreeRTOS, is ST planning to support integration of for FreeRTOS-Plus-TCP into the IDE/Mx?There are minimal examples available for setting up this addon making it extremely ...
From my research, I've read that LwIP is written with FreeRTOS, but can be altered to support any OS. Since ST has made an effort to support/encourage LwIP and ThreadX, are there any resources/examples that we can reference?I am doing my evaluation w...
I am trying to prototype ethernet on the NUCLEO-H7S3L8 eval board. When enabling ethernet through CubeMx using the same configuration I've used on the NUCLEO-H563ZI, the ethernet driver fails initialization. Is there an alternative Ethernet driver th...
I have a NUCLEO-H7S3L8 board, and I am unable to debug any of the projects. I receive a sigtrap error upon debugging. I have tried multiple projects in ST's Github. STM32CubeH7RS/Projects/NUCLEO-H7S3L8 at main · STMicroelectronics/STM32CubeH7RSAll pr...
1. Does the STM32MP157D-DK1 board have 3.0 USB ports? Does the USB C connector have USB 3.0 capabilities?2. If no to the questions above, what STM32MP board should we use if we want to have USB 3.0 capabilities?
Kudos from