Skip to main content
Associate
January 2, 2025
Question

System gets stuck in hardfault handler after sending few chunks with LWIP using FreeRTOS

  • January 2, 2025
  • 3 replies
  • 1434 views

HELLO, 
I’m facing a hard fault when transmitting large data (60,018 bytes) via LwIP TCP/IP on STM32H723 with FreeRTOS. After increasing buffers and adjusting lwipopts.h, only 4000-5000 bytes transmit successfully. Remaining data causes crashes, likely due to memory exhaustion, stack overflow, or incorrect buffer handling. Need help resolving this.

HARD FAULT STACK-
"cam_bsnet Debug [STM32 C/C++ Application]
cam_bsnet.elf [cores: 0]
Thread #1 [main] 1 [core: 0] (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)
HardFault_Handler() at stm32h7xx_it.c:113 0x8002070
<signal handler called>() at 0xfffffffd
ethernet_input() at ethernet.c:113 0x8023328
tcpip_thread_handle_msg() at tcpip.c:174 0x801714e
tcpip_thread() at tcpip.c:148 0x8017102
pxPortInitialiseStack() at port.c:214 0x8012ab0
arm-none-eabi-gdb (13.2.90.20230627)
ST-LINK (ST-LINK GDB server)"

THANKS IN ADVANCE

This topic has been closed for replies.

3 replies

TDK
January 2, 2025

Probably overflowing the stack, or heap and stack are colliding. Look at the line that triggers failure (ethernet.c:113) and see where the buffer is being stored and verify it's not overwriting anything.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ArushAuthor
Associate
January 3, 2025

thanks, I did the changes suggested by you, now i am able to transmit the complete data but sometimes system gets stuck in Hard Fault Handler during start, i think there is some issue in "pxPortInitialiseStack() at port.c:214 0x8011334"-
Hard Fault Stack-

cam_bsnet Debug [STM32 C/C++ Application]
cam_bsnet.elf [cores: 0]
Thread #1 [main] 1 [core: 0] (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)
HardFault_Handler() at stm32h7xx_it.c:112 0x8001e2c
<signal handler called>() at 0xfffffffd
ethernet_input() at ethernet.c:113 0x8021bb4
tcpip_thread_handle_msg() at tcpip.c:174 0x80159d6
tcpip_thread() at tcpip.c:148 0x801598a
pxPortInitialiseStack() at port.c:214 0x8011334
arm-none-eabi-gdb (13.2.90.20230627)
ST-LINK (ST-LINK GDB server)
Need help resolving this.
ST Employee
February 17, 2025

Hello @Arush ,

it seems that you are lacking proper buffer management, so you are running out of stack.

this is worth mentioning about LwIP memory management:

  • LwIP provides a flexible way to manage memory pool sizes and organization.
  • It reserves a fixed-size static memory area in the data segment. It is subdivided into the various pools that lwIP uses for the various data structures. As an example, there is a pool for struct tcp_pcb, and another pool for struct udp_pcb. Each pool can be configured to hold a fixed number of data structures. This number can be changed in the lwipopts.h file. For example, MEMP_NUM_TCP_PCB and MEMP_NUM_UDP_PCB define the maximum number of tcp_pcb and udb_pcb structures that can be active in the system at a given time.
  • The user options can be changed in lwipopts.h

Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.