User Activity

Hi together,I have some errors and bugs that I have when generating code from the STM32CubeMX (V6.14.0) (STM32CubeIDE V1.18.0) on Windows11 as well as with the graphical interface.1. STM32CubeIDE/MX generates the function PeriphCommonClock_Config() i...
Hi,I am using the STM32H7R7I8T6 in combination with the Macronix MX25L12833F on a custom board. As I understand it, I need to configure the External Memory Manager and the XSPI interface in STM32CubeMX and after initializing the flash via SFDP, the b...