STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

1.18.0/.1 GDB server error

Hello all.Personal emotional outburst (just jump it if you don't work for stm):I can't understand how it's possibile, but every single time I trust STM and go for an update, everything stops working and I have to loose hours of my life trying to fix ...

CZamb.2 by Associate II
  • 1368 Views
  • 2 replies
  • 0 kudos

LTDC Display Type Restriction

I am using the STM32H743VIT and trying to integrate using LTDC. The Display Type options in CUBEMX only allow 16 or 18 bit RGB. I know there is no LTDC_R0, so I assume that is why there is not option for 24 bit RGB; however, we were just planning on ...

16384 points of FFT(Fast Fourier Transform)

Hello community, In my project requires upto 16384 points of FFT(Fast Fourier Transform) . I found out that I can’t perform this number of FFT points using arm CMSIS DSP library since it is limited to 4096 point Max. Due to this I have to use externa...

SA  V.1 by Senior
  • 7213 Views
  • 15 replies
  • 6 kudos

Resolved! Timer to DMA to SPI STM32H723 using LL

Hi,I want a GPIO pin to trigger an SPI transfer. The way that I have figured this should work is:PG3 -> TIM23 -> DMA2 -> SPI1 Here is basically what I have so far:/* Includes ---------------------------------------------------------------------------...

ZacJFrank by Associate II
  • 1915 Views
  • 5 replies
  • 0 kudos