STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LWIP 2 interfaces issue

Dear colleagues, hello! Question about LWIP. I have two network interfaces, one on the QCA 7000 chip via SPI, the second on LAN 8742, installed on the debug board. I use the Socket API. The problem is as follows: The server is running on one interfac...

Ivan4S4 by Associate II
  • 2718 Views
  • 9 replies
  • 2 kudos

CubeIDE arm-none-eabi-gcc Toolchain sources

Hi,I am currently working on a build container for my project and I’m using the ARM toolchain (arm-none-eabi-gcc) from ARM Developer sources:  https://developer.arm.com/downloads/-/arm-gnu-toolchain-downloads .Do you have an authless link that provid...

lotou by Associate II
  • 4045 Views
  • 1 replies
  • 2 kudos

FLASH_TYPEPROGRAM_FAST fails in G0B1

I tried to use FLASH_TYPEPROGRAM_FAST in a G0B1 but is not working after a page erase. I suppose it will work with mass erase but not tried. Only works FLASH_TYPEPROGRAM_DOUBLEWORD. I've also tried to make my own function to write only 32bits modifin...

stm32h7s78-dk how to run FATfs Multi Access

Hi Team,I'm trying to run Fatfs Multi Access example in the stm32h7s78-dk. Im having hard time understanding the Readme instructions.  I have the switch set to boot0.Im using stmcube progrmamer. I have added external loader: MX66UW1G45G_STM32H7S78-DK...

ropodi17 by Associate II
  • 1295 Views
  • 2 replies
  • 1 kudos

Resolved! Bug on fatfs

Hello.I'm using Riverdi board.This board uses STM32H757XIH6 .I used FATFS R0.12c with uSD and USB-MassStorage in Unicode mode When mount uSD and then USB I noticed that FatFs[0] is overwritten.  

MauFanGilaMedical_0-1745909669577.png

SD Card + FATFS USB MSC data Corruption Issue

Originally posted in TouchGFX Forum - moved & merged with duplicate.Hi,I am working on the STM32F439 development board. I am creating a test.csv file and logging data using FATFS on an SDIO SD card. I can view the data through USB MSC on a Windows PC...

pankaj4 by Associate II
  • 2214 Views
  • 5 replies
  • 1 kudos