cancel
Showing results for 
Search instead for 
Did you mean: 

DMA for Quadtrature Encoder not working (stm32g0x1)

shadj
Associate

I am working with a Quadrature Encoder that uses TIM2 (encoder mode). The encoder mode automatically captures an increase in the register htim2.Instance->CNT

I am trying to use DMA to fill a buffer with the CNT values however it does not seem to work. 

I would really appreciate any help!

My relevant code: 

 

initializations: 
 TIM_HandleTypeDef htim2;
 TIM_HandleTypeDef htim3;
 TIM_HandleTypeDef htim16;
 DMA_HandleTypeDef hdma_tim16_com;

 int32_t count_buf[COUNT_BUF_CAPACITY];

main: 

  MX_DMA_Init();
  MX_TIM2_Init();
  MX_TIM16_Init();

  HAL_TIM_Base_Start_IT(&htim16);
  HAL_TIM_Encoder_Start_IT(&htim2, TIM_CHANNEL_ALL);

  HAL_DMA_Start(&hdma_tim16_com,&htim2.Instance->CNT,count_buf,4);


static void MX_DMA_Init(void)
{

  /* DMA controller clock enable */
  __HAL_RCC_DMA2_CLK_ENABLE();

  /* DMA interrupt init */
  /* DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn);

}

static void MX_TIM16_Init(void)
{

  /* USER CODE BEGIN TIM16_Init 0 */

  /* USER CODE END TIM16_Init 0 */

  /* USER CODE BEGIN TIM16_Init 1 */

  /* USER CODE END TIM16_Init 1 */
  htim16.Instance = TIM16;
  htim16.Init.Prescaler = 63;
  htim16.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim16.Init.Period = 99;
  htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim16.Init.RepetitionCounter = 0;
  htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
  if (HAL_TIM_Base_Init(&htim16) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM16_Init 2 */

  /* USER CODE END TIM16_Init 2 */

}

static void MX_TIM2_Init(void)
{

  /* USER CODE BEGIN TIM2_Init 0 */

  /* USER CODE END TIM2_Init 0 */

  TIM_Encoder_InitTypeDef sConfig = {0};
  TIM_MasterConfigTypeDef sMasterConfig = {0};

  /* USER CODE BEGIN TIM2_Init 1 */

  /* USER CODE END TIM2_Init 1 */
  htim2.Instance = TIM2;
  htim2.Init.Prescaler = 0;
  htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim2.Init.Period = 4294967295;
  htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
  sConfig.EncoderMode = TIM_ENCODERMODE_TI12;
  sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;
  sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;
  sConfig.IC1Prescaler = TIM_ICPSC_DIV1;
  sConfig.IC1Filter = 0;
  sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;
  sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;
  sConfig.IC2Prescaler = TIM_ICPSC_DIV1;
  sConfig.IC2Filter = 0;
  if (HAL_TIM_Encoder_Init(&htim2, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM2_Init 2 */

  /* USER CODE END TIM2_Init 2 */

}

 

 

3 REPLIES 3
Uwe Bonnes
Chief

What is your intention? What use is information that the encoder has changed? Normally you sample the encoder when you need to process the actual value and also at a slow rate so no overflow happens.
Otherwise, not looking at your code:
- What event should trigger the DMA transfer from encoder counter to the dma memory?

Thank you for the reply. 

My intention is to update a buffer, from the CNT register using DMA. It should not occur based on a specific event, it should always read the value of the register.

You need some event to trigger a DMA transaction. What about setting up an EXTI interrupt on one of the decoder pins and transfer in the interrupt routine?