STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32N6 VENC at lower resolutions

Hi everyone,I have successfully deployed the VENC_SDCARD example on the board and can see its feed on my laptop. Now, I want to record it at 480x480 resolution instead of the default 800x480 provided in the example.I have modified the buffer size, DC...

Image (1).jpeg Screenshot from 2025-07-15 13-41-14.png

Clock / Timing problem in I2C

I am trying to run a loopback test with 2 i2c's on the same board. The onboard leds need to light up on successful transmission and reception, the problem is the leds light up when in debug mode, going line by line, but not in stand#define I2C1_ADD (...

maya16 by Associate III
  • 624 Views
  • 3 replies
  • 1 kudos

Resolved! Timer PWM with DMA stops too early on STM32G431

Hi there,I would like to control WS2812B LEDs with a PWM timer and DMA.There are various tutorials on this, but they have not helped me and I am now asking you. Because it requires slightly different configurations depending on the model (F3, F4, G4,...

tim1_mode.png tim1_conf1.png tim1_conf2.png dma_settings.png
ABach.4 by Associate II
  • 2536 Views
  • 12 replies
  • 0 kudos