cancel
Showing results for 
Search instead for 
Did you mean: 

MORE BUGS STMCubeMX migration to v6.13 FW H7 V1.12 - ETH HAL

mbarg.1
Lead

After experiencing more problems in legacy codes, we found that STM changed HAL drivers without any notice.

THIS CAN BE BLOCKING.

Example : 

((uint32_t)((pFilterConfig->BroadcastFilter == DISABLE) ? 1U : 0U) << 5) |

is NOW

((uint32_t)((pFilterConfig->BroadcastFilter == ENABLE) ? 1U : 0U) << 5) |

in

HAL_ETH_SetMACFilterConfig()

Only workaround:

SPEND all the time it needs and check all drivers carefully for changes.

stm32h7xx_hal_eth.c has dozen of changes, impossible to compare files and get differences easily.

 

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

Escalated internally for analysis. Internal ticket number: 197721 

Thank you for your contribution.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
milorad
Associate III

In the same context, if the functionality of a setting (BroadcastFilter) is reversed how would the code that relied on the old functionality be able to handle that?
Also, this change is now present in some of the newly updated HALs, what about HALs for older families (even obsolete ones) that will probably never be updated?

mbarg.1
Lead

FW H7 V1.12.1 solves the bug

BUT once more, in release notes there is NO indication of this fix.