STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB CDC using USBX on F411

I am just a bit confused about how the CDC examples using USBX work. In the sample I've seen it seems that the code sets up some sort of UART to USB bridge. I think I don't need the UART and wanted to send and process data like the classic library us...

Use STM32H750 Internal Flash

I'm using STM32H750Is it possible to read and write like EEPROM in a specific part of the program (the last part of the internal flash area?)?I think it's impossible because there's only one sectorIf possible, I would appreciate it if you could give ...

SMj.1 by Associate II
  • 692 Views
  • 4 replies
  • 2 kudos

Resolved! USB CDC in STM32H563

tried to set up a USB device serial emulation (CDC) for STM32H563. Started a Free RTOS based project project in STM32CubeMX. But there I only can activate USB as "device_only in the "connectivity" segment but do not find any other USB related setting...

VKoen.1 by Associate II
  • 2516 Views
  • 4 replies
  • 0 kudos

STM32N6570-DK: LCD flickers when boot from flash

Hello,I have an application that shows image from camera from time to time on the screen. This app flashed at 0x7010'0000 and works well when I run FSBL in dev mode from debugger.But if I flash this FSBL at 0x7000'0000 and switch to flash boot app wo...

p5n by Associate II
  • 816 Views
  • 4 replies
  • 0 kudos

Resolved! X-CUBE-LED1642 download

The X-CUBE-LED1642 software seems to have gone missing. There are no links on the web page where you can download it.Should be here: https://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32c...

qua by Senior
  • 515 Views
  • 1 replies
  • 0 kudos

STM32H743 ETH Problem with RT Thread and LWIP

Hi,I created the STM32H743 project based on RT Thread and LWIP, only open ICache, if I modify the content of a function, it will lead to the Ethernet transmission success, but there is no data on the MII interface, debugging compared the ETH register...

ketlen by Associate II
  • 1410 Views
  • 7 replies
  • 3 kudos

Resolved! Update about USB PD Stack to support EPR mode

Any update on when the middleware will be extended to support EPR? The availability of TCPPE or devkits is not really all that important for a software update and probably should not be gating. Should I switch to the HUSB238A instead of the STM32G0?

zbrozek by Associate II
  • 678 Views
  • 1 replies
  • 0 kudos