cancel
Showing results for 
Search instead for 
Did you mean: 

STM32's TIM triggers SPI's DMA sends MSSI when using NSS

Pangzi
Associate

Edit by ST Moderator: This post has been translated from Chinese to comply with the ST Community Terms and Conditions (§10.2).

STM32's TIM triggers SPI's DMA send using NSS when MSSI is used
Using stm32h743, timer TIM12 enable event, spi1 enable NSS, set MSSI to 15 to enable cyclic sending of DMA for SPI and select TRGO of TIM12 as trigger source.


STM32的TIM触发SPI的DMA发送使用NSS时MSSI的问题
使用stm32h743,定时器TIM12使能事件,spi1使能NSS,将MSSI设置为15,使能SPI的DMA的循环发送,并将触发源选择TIM12的TRGO。

Pangzi_1-1743407784000.pngPangzi_2-1743407800941.png

Pangzi_3-1743407814063.png

The MSSI has an effect when only the first data sent is delayed during the phenomenon, and none of the later ones have an effect.
现象时只有第一个发送的数据会有延时,MSSI有效果,后面的都没有效果。

Pangzi_4-1743407859340.png

 

1 REPLY 1
Sarra.S
ST Employee

Hello @Pangzi

This is normal behavior. The MSSI is designed to introduce a delay between the NSS signal and the start of the clock for the first transfer, so the delay is only applied at the beginning of the transfer, as you have observed. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.