STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB OTG Phy

Hi allFor some reason unknown to me, my PHYSEL bit in GUSBCFG is not setting, and I don't know why static inline void core_initialisation(void) //from page 3403 { // 1. Program OTG_GAHBCFG register: // - Enable global interrupt mask bit (GINT...

Maaz1 by Associate III
  • 747 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 FFT USING CMSIS DSP -1024Point FFT

I need to do a 1024 point FFT on the STM32F446RE Eval Board. I try to integrate the CMSIS-DSP Libraries as mentioned in the forum and it creates errors only and I can't even run the program. I need to do a q15 FFT ,but it is not working. Help me to t...

STM.png

LwIP Custom memory pool configuration

I'm working on building an Ethernet infrastructure using LWIP on an STM32H7 series MCU for various purposes. In this setup, I want to avoid using malloc, and instead rely entirely on LWIP’s memory pool system for all memory allocations. Here's the co...

SSone.1 by Associate III
  • 1285 Views
  • 1 replies
  • 1 kudos

PWR_STANDBY_RTC example in Nucleo Board G474RE

I have tried to measurement the current consumption in standby mode but it is too high. I am using the example "PWR_STANDBY_RTC" listed in AN5315, STM32Cube firmware examples for STM32G4 Series which should work in Nucleo Board G474RE. The values I o...

Magera by Associate II
  • 921 Views
  • 2 replies
  • 0 kudos

FreeRTOS - USB CDC not working with USART1

Moved from this discussion as it's linked to the embedded software USB and FreeRTOS. My problem has always been that when USB and USART1 are working at the same time, USB as a virtual serial port is not working properly. In my code, two different thr...

jack_wang by Associate II
  • 1201 Views
  • 4 replies
  • 0 kudos