STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Question about TouchSensing

Greetings, I have a question about the touchsensing module. I am using a stm32u585rit6 mcu in a custom-made board and making a project using azure rtos. I needed to add touchsensing. I watched the app_azure_rtos_config.h and noticed that there is sta...

STM32H7S78-DK USB hangs in init

Hello, I am trying to utilize the USB peripheral in STM32cubeIDE with the STM32H7S78-DK. It hangs forever in MX_USB_INIT on a function USB CORE RESET. With FS and HS this same issue seems to be happening. Pictures show config in the GUI and the afore...

mtc65536 by Associate II
  • 1475 Views
  • 9 replies
  • 0 kudos

Resolved! Simple DAC control appears not simple

    Dear supporters,In a project I want to create a feedback mechanism to keep the top of a pulse-shaped signal between boundaries. Most of this seems working, except the control of the DAC channel, that should output a voltage for the diode-laser wh...

FredS by Senior
  • 1366 Views
  • 9 replies
  • 1 kudos

STM32H7 Flash RCC Problem

Hi,When I was using the STM32H743ZI chip, I set the system frequency of the chip to 160 MHz. Only enable the ICache, do not enable the DCache and the MPU.According to the prompt from CubeMX, the maximum peripheral clock is 240 MHz. Therefore, I confi...

ketlen_0-1754647199964.png ketlen_1-1754647618262.png ketlen_2-1754647635564.png ketlen_3-1754648396445.png
ketlen by Associate II
  • 843 Views
  • 3 replies
  • 0 kudos

Resolved! STMG07 Uart Config after exit System Bootload

Hi,I have an issue with the UASRT communication being abnormal.First case:Access System Bootload Mode by Options bytesAccess the Main Application by the UART protocol ( UART2)Send the first UART packet to the ST MCU via UART2 that contains the UART e...

TesterSAM by Associate III
  • 792 Views
  • 6 replies
  • 0 kudos

Issue with memory sharing between cores

Hi Team, I'm new to STM32H7 controller. I've started exploring the shared memory in this dual core controller. I found a great one from MAJERLE. Thanks for that. I used the same concept and made a Flag to check for new data to read and write, it was ...