cancel
Showing results for 
Search instead for 
Did you mean: 

Question about TouchSensing

j_filipe
Senior

Greetings, 
I have a question about the touchsensing module. I am using a stm32u585rit6 mcu in a custom-made board and making a project using azure rtos. I needed to add touchsensing. I watched the app_azure_rtos_config.h and noticed that there is static memory allocation via threadX memory pools (#define TOUCHSENSING_APP_MEM_POOL_SIZE   5000). Then, at the app_azure_rtos.c file there is the following: 

__ALIGN_BEGIN static UCHAR  tsc_byte_pool_buffer[TOUCHSENSING_APP_MEM_POOL_SIZE] __ALIGN_END;
static TX_BYTE_POOL tsc_app_byte_pool;

if (tx_byte_pool_create(&tsc_app_byte_pool, "TOUCHSENSING App memory pool", tsc_byte_pool_buffer, TOUCHSENSING_APP_MEM_POOL_SIZE) != TX_SUCCESS)
  {
    /* USER CODE BEGIN TOUCHSENSING_Byte_Pool_Error */

    /* USER CODE END TOUCHSENSING_Byte_Pool_Error */
  }
  else
  {
    /* USER CODE BEGIN TOUCHSENSING_Byte_Pool_Success */

    /* USER CODE END TOUCHSENSING_Byte_Pool_Success */

    memory_ptr = (VOID *)&tsc_app_byte_pool;
    status = MX_TOUCHSENSING_Init(memory_ptr);
    if (status != TSL_STATUS_OK)
    {
      /* USER CODE BEGIN  MX_TOUCHSENSING_Init_Error */
      while(1)
      {
      }
      /* USER CODE END  MX_TOUCHSENSING_Init_Error */
    }
    /* USER CODE BEGIN  MX_TOUCHSENSING_Init */

    /* USER CODE END  MX_TOUCHSENSING_Init */
  }

 

What is the purpose of this memory pool? Is there any thread related to touchsensing running?
Thank you! 

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @j_filipe ,

The memory pool in the TouchSensing module is used to reserve a specific memory space for the middleware (MW) functions of the TouchSensing module.
TOUCHSENSING_APP_MEM_POOL_SIZE is generated "hardcoded" by CubeMX. When you have ThreadX + TouchSensing MW, it will add this define, with the default value 5000 in the app_azure_rtos_config.h file, and you can change it manually in the code if needed.
The define itself is used to create the tsc_byte_pool_buffer, used for the memory context of the TouchSensing MW functions.
This "buffer" is a memory space reserved for the MW, so it is not really "used" by the MW directly.
I'll suggest having a look at the official documentation regarding that point:
https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/threadx/chapter3.md#memory-block-pools

The TouchSensing MW entry point is managed by function "MX_TOUCHSENSING_Init()", and is working in this memory pool.

Hope my answer helps you!

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @j_filipe ,

The memory pool in the TouchSensing module is used to reserve a specific memory space for the middleware (MW) functions of the TouchSensing module.
TOUCHSENSING_APP_MEM_POOL_SIZE is generated "hardcoded" by CubeMX. When you have ThreadX + TouchSensing MW, it will add this define, with the default value 5000 in the app_azure_rtos_config.h file, and you can change it manually in the code if needed.
The define itself is used to create the tsc_byte_pool_buffer, used for the memory context of the TouchSensing MW functions.
This "buffer" is a memory space reserved for the MW, so it is not really "used" by the MW directly.
I'll suggest having a look at the official documentation regarding that point:
https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/threadx/chapter3.md#memory-block-pools

The TouchSensing MW entry point is managed by function "MX_TOUCHSENSING_Init()", and is working in this memory pool.

Hope my answer helps you!

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Thank you for the input!