STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FreeRTOS Hard Fault issue

NUCLEO F411RE I'm checking to see if I've got FreeRTOS integrated properly. So I've set up 2 tasks each with their own counter. In debug I was expecting to see the counter for Task1 to count up whilst Task2 never gets updated.When I step through the ...

Resolved! USBX Device MSC in Standalone mode

I'm trying to get USBX Device MSC to work in Standalone mode (without RTOS).  I loosely followed @B.Montanari 's example in https://community.st.com/t5/stm32-mcus/how-to-implement-usbx-in-standalone-mode/ta-p/614435, and also referred to a CubeMX exa...

PRuss by Associate II
  • 6316 Views
  • 7 replies
  • 7 kudos

STM32F429I-discovery Purple screen

Hello. This is my first week with MCU's. I choose STM and want to stick with it. But it makes only pain :) So I was able to make some GPIO to work but have a complete disaster with LCD. The board came with some demo firm, and it was erased. So I am d...

grisom13 by Associate III
  • 1064 Views
  • 7 replies
  • 1 kudos

Resolved! USB CoreReset stuck at count

Hi all static HAL_StatusTypeDef USB_CoreReset(USB_OTG_GlobalTypeDef *USBx) { __IO uint32_t count = 0U; /* Wait for AHB master IDLE state. */ do { count++; if (count > HAL_USB_TIMEOUT) { return HAL_TIMEOUT; } } while ...

Maaz1 by Associate III
  • 460 Views
  • 1 replies
  • 0 kudos

Resolved! Question about TouchSensing

Greetings, I have a question about the touchsensing module. I am using a stm32u585rit6 mcu in a custom-made board and making a project using azure rtos. I needed to add touchsensing. I watched the app_azure_rtos_config.h and noticed that there is sta...

STM32H7S78-DK USB hangs in init

Hello, I am trying to utilize the USB peripheral in STM32cubeIDE with the STM32H7S78-DK. It hangs forever in MX_USB_INIT on a function USB CORE RESET. With FS and HS this same issue seems to be happening. Pictures show config in the GUI and the afore...

mtc65536 by Associate II
  • 1373 Views
  • 9 replies
  • 0 kudos