User Activity

Hi, I'm trying to use https://www.st.com/en/embedded-software/x-cube-eeprom.html on my custom stm32g030 board.Following the examples I write this code:   HAL_FLASH_Unlock(); ee_status = EE_Init(EE_FORCED_ERASE); if(ee_status != EE_OK) { Erro...
Hi, erasing a complete page (2KB) to just write a few bytes is a waste of erase/write cycle. Is there a way to write data in differents part of the page each time? when there is no more space then a page erase should be fired and start over. Is there...
Hi, I'm working with a stm32f722 and a ublox f9p gps. I just have 2 ubx messages. One with 36 bytes long and the other with 72 bytes. They income with a variable interval between them (a couple of byte time at most, usually they come together). This ...
Hi, I would like to use cubeide (MX tool) to generate a project that use EXTI_13 but with IRQ disabled by default. I can choose Enable/Disable (generate all code or none), Create code on MSPInit function or in MX_NVIC_Init, call HAL_GPIO_EXTI_IRQHand...
Hi, I have a sensor that send data over uart to a stm32f722 uC. This sensor is powered at the same time of uC. I've noticed that some times the sensor stop sending data. For example, if the code is running ok and then reboot the uC some times the sen...