Skip to main content
Will_Robertson
Associate III
December 27, 2024
Question

STM32N6 - Video Capture from MIPI CSI-2 Image Sensor (Sony, ST BrightSense)

  • December 27, 2024
  • 2 replies
  • 2812 views

Hi,

I was wondering if there's any reference application or if you have any advice on drivers to capture video from a MIPI CSI-2 image sensor (perhaps Sony or the ST BrightSense image sensors (VB1940 (active) or VD1940 (preview) match the 5.1 MP dimensioning of the STM32N6) with STM32N6x7 or STM32N6x5 μCs?

The aim would be to waken up the STM32N6 in response to an external digital input, record video from a MIPI CSI-2 image sensor to SD or eMMC then return to sleep mode.

I'd be happy to consider bare metal, Zephyr or FreeRTOS - whatever you recommend.

Thank you very much for your help and all the best for 2025!

Will

2 replies

RomainR.
ST Employee
December 28, 2024

Hello @Will_Robertson 

You can refer to the following examples project using Sony IMX335 5MPx CMOS camera with CSI.
These demos also use VENC. 

Bare metal version:
STM32Cube_FW_N6_V1.0.0\Projects\STM32N6570-DK\Applications\VENC\VENC_SDCard

ThreadX version:
STM32Cube_FW_N6_V1.0.0\Projects\STM32N6570-DK\Applications\VENC\VENC_SDCard_ThreadX

Best regards,

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Will_Robertson
Associate III
December 28, 2024

Hi @RomainR. 

Thank you very much - that's an enormous help to me learning to use CSI cameras and VENC with the STM32N6!

Thank you also for the ThreadX example - ThreadX could be very valuable to our application.

https://wiki.st.com/stm32mcu/wiki/ISP:Getting_started_with_X-CUBE-ISP#Change_the_camera_module says

"The software is natively compatible with the MB1854B IMX335 and STEVAL-66GYMAI VD66GY camera modules. Simply change the camera module and restart the software. No software reconfiguration is needed."

"For a customer camera module, the sensor driver must be added to the camera middleware and a first tuning must be performed using the STM32 ISP IQTune desktop application to generate the final isp_param_conf.h file that can then be updated."

In practice, how difficult is it to find and add the sensor drives for other ST and Sony image sensors?

Thank you very much for your help!

Will

RomainR.
ST Employee
December 28, 2024

Hi @Will_Robertson 

Hard to say but for each image sensor there is necessarily a low level driver to implement. Which requires reading the different datasheets to correctly configure the protocol.
What I can tell you about the VD66GY is that it should be integrated into the next versions of the X-CUBE-IPS, I can't give you an official date for now.

Best regards,

Romain

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
March 3, 2026

Hello @Will_Robertson I want to quickly catch-up with you about this project: how is the implementation with Zephyr, have you perhaps gathered some experience with programming such MIPI CSI-2 interfaces with Zephyr RTOS?

Thank you

Kind regards