Skip to main content
Associate II
December 21, 2024
Question

STM32G491 does not start from RAM (in debug mode) - External loader problem

Hi,

I am working on an external loader for STM32G491.
For STM32F4 series microcontroller, everything works fine, but STM32G491 does not work.
I observed that the external loader program is loaded into RAM, but does not execute.
I did some tests with running the program from RAM in debug mode.
I observed that if the FLASH memory is erased then the program loaded into RAM does not want to start (see image below).


If there is any previous running program in FLASH memory, then loading the test program into RAM and running it with the debugger works fine.
For STM32F4 series microcontroller, I can always run the program from RAM ( also for deleted FLASH memory - which seems to be normal).

The problem with the external loader is that the debugger initially deletes the processor's FLASH memory, then using the external loader to erase the external memory, but the external loader no longer works, because the FLASH memory is deleted.

I use CubeIDE Version: 1.14.0  &  HAL library

 

LehuW_1-1734817470428.png

 

 

 Start of the linker file:

 

/* Entry Point */
ENTRY(Init)

/* Generate 2 segment for Loader code and device info */
PHDRS {Loader PT_LOAD ; SgInfo PT_LOAD ; }

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x200 ; /* required amount of heap */
_Min_Stack_Size = 0x400 ; /* required amount of stack */

/* Specify the memory areas */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000004, LENGTH = 112K
}

 

 

 

What did I miss?
Any ideas?

 

Best regards,

Lehu

 

 

This topic has been closed for replies.

11 replies

ST Technical Moderator
December 23, 2024

Hello @LehuW 

Could you share with us the source code please? 

Is the code in internal flash initialize the external flash?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
LehuWAuthor
Associate II
December 23, 2024

I did some additional tests.

I think the main problem is on the side of the ST-LINK programmer.
I have a log of the programming process.

At the beginning the FLASH memory of the processor is erased - address 0x8000000.
From address 0x20000004 the debugger loads 0x000007A0 bytes of the loader with which it will erase the internal FLASH memory.
Next sets PC 0x20000005 and starts the erase procedure.
Next proceeds to erase the external flash memory.

Next loader starts to erase external mamory.  (Erasing Segment <1> Address <0x90000000> Size <37>Bytes)

Sets PC 0x200006C1 and starts erasing.

But what is at address 0x200006C1 ?
The external loader has not been loaded.

From .map file we know that the Init() function of the external loader is at address 0x200006C1 (.text.Init 0x00000000200006c0 0x88 ./Core/Src/Loader_Src.o), but it has not been loaded.

[6.621] spawnCubeProgrammer(): 18:39:39:779 Memory Programming ...
[6.621] spawnCubeProgrammer(): 18:39:39:779 Opening and parsing file: ST-LINK_GDB_server_a05132.srec
[6.621] spawnCubeProgrammer(): 18:39:39:780 File : ST-LINK_GDB_server_a05132.srec
[6.621] spawnCubeProgrammer(): 18:39:39:780 Size : 7.56 KB 
[6.621] spawnCubeProgrammer(): 18:39:39:780 Address : 0x08000000 
[6.621] spawnCubeProgrammer(): 18:39:39:780 
[6.621] spawnCubeProgrammer(): 
[6.621] spawnCubeProgrammer(): 18:39:39:780 Erasing Segment <0> Address <0x08000000> Size <7708>Bytes
[6.621] spawnCubeProgrammer(): 18:39:39:780 Erasing memory corresponding to segment 0:
[6.621] spawnCubeProgrammer(): 18:39:39:780 Memory Erase via FlashLoader!
[6.621] spawnCubeProgrammer(): 18:39:39:780 Memory erase...
[6.621] spawnCubeProgrammer(): 18:39:39:782 halt ap 0 
[6.621] spawnCubeProgrammer(): 18:39:39:782 w ap 0 reg 15 PC (0x20000000) 
[6.621] spawnCubeProgrammer(): 18:39:39:782 w ap 0 reg 17 MSP (0x20000500) 
[6.621] spawnCubeProgrammer(): 18:39:39:783 w ap 0 reg 16 xPSR (0x01000000) 
[6.621] spawnCubeProgrammer(): 18:39:39:785 w ap 0 @0x20000BE0 : 0x00000200 bytes, Data 0x00000000...
[6.621] spawnCubeProgrammer(): 18:39:39:785 w ap 0 @0x20000000 : 0x00000004 bytes, Data 0x0000BE00...
[6.621] spawnCubeProgrammer(): 18:39:39:787 w ap 0 @0x20000004 : 0x000007A0 bytes, Data 0xF000B580...
[6.621] spawnCubeProgrammer(): 18:39:39:789 Erasing internal memory sectors [0 3]
[6.621] spawnCubeProgrammer(): 18:39:39:789 Init flashloader...
[6.621] spawnCubeProgrammer(): 18:39:39:790 halt ap 0 
[6.621] spawnCubeProgrammer(): 18:39:39:790 w ap 0 reg 0 R0 0x00000001
[6.621] spawnCubeProgrammer(): 18:39:39:790 w ap 0 reg 1 R1 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:790 w ap 0 reg 2 R2 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:790 w ap 0 reg 3 R3 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:790 w ap 0 reg 4 R4 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:791 w ap 0 reg 5 R5 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:791 w ap 0 reg 6 R6 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:791 w ap 0 reg 7 R7 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:792 w ap 0 reg 8 R8 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:792 w ap 0 reg 9 R9 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:792 w ap 0 reg 10 R10 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:792 w ap 0 reg 11 R11 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:792 w ap 0 reg 12 R12 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:793 w ap 0 reg 13 SP 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:793 w ap 0 reg 14 LR 0x20000001
[6.621] spawnCubeProgrammer(): 18:39:39:793 w ap 0 reg 15 PC 0x20000005
[6.621] spawnCubeProgrammer(): 18:39:39:793 w ap 0 reg 16 xPSR 0x01000000
[6.621] spawnCubeProgrammer(): 18:39:39:793 w ap 0 reg 17 MSP 0x20000BA0
[6.621] spawnCubeProgrammer(): 18:39:39:793 w ap 0 reg 18 PSP 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:793 run ap 0 
[6.621] spawnCubeProgrammer(): 18:39:39:794 halt ap 0 
[6.621] spawnCubeProgrammer(): 18:39:39:794 r ap 0 reg 0 R0 0x00000001
[6.621] spawnCubeProgrammer(): 18:39:39:794 Loader sector erase...
[6.621] spawnCubeProgrammer(): 18:39:39:794 w ap 0 reg 0 R0 0x08000000
[6.621] spawnCubeProgrammer(): 18:39:39:795 w ap 0 reg 1 R1 0x08001800
[6.621] spawnCubeProgrammer(): 18:39:39:795 w ap 0 reg 2 R2 0x00000002
[6.621] spawnCubeProgrammer(): 18:39:39:795 w ap 0 reg 3 R3 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:795 w ap 0 reg 4 R4 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:795 w ap 0 reg 5 R5 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:796 w ap 0 reg 6 R6 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:796 w ap 0 reg 7 R7 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:796 w ap 0 reg 8 R8 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:796 w ap 0 reg 9 R9 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:797 w ap 0 reg 10 R10 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:797 w ap 0 reg 11 R11 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:797 w ap 0 reg 12 R12 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:797 w ap 0 reg 13 SP 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:797 w ap 0 reg 14 LR 0x20000001
[6.621] spawnCubeProgrammer(): 18:39:39:798 w ap 0 reg 15 PC 0x2000038B
[6.621] spawnCubeProgrammer(): 18:39:39:798 w ap 0 reg 16 xPSR 0x01000000
[6.621] spawnCubeProgrammer(): 18:39:39:798 w ap 0 reg 17 MSP 0x20000BA0
[6.621] spawnCubeProgrammer(): 18:39:39:798 w ap 0 reg 18 PSP 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:798 run ap 0 
[6.621] spawnCubeProgrammer(): 18:39:39:886 halt ap 0 
[6.621] spawnCubeProgrammer(): 18:39:39:886 r ap 0 reg 0 R0 0x00000001
[6.621] spawnCubeProgrammer(): 18:39:39:886 erase: 0106ms
[6.621] spawnCubeProgrammer(): 18:39:39:886 Erasing Segment <1> Address <0x90000000> Size <37>Bytes
[6.621] spawnCubeProgrammer(): 18:39:39:886 Erasing memory corresponding to segment 1:
[6.621] spawnCubeProgrammer(): 18:39:39:886 Memory Erase via FlashLoader!
[6.621] spawnCubeProgrammer(): 18:39:39:886 Memory erase...
[6.621] spawnCubeProgrammer(): 18:39:39:888 halt ap 0 
[6.621] spawnCubeProgrammer(): 18:39:39:888 w ap 0 reg 15 PC (0x20000000) 
[6.621] spawnCubeProgrammer(): 18:39:39:889 w ap 0 reg 17 MSP (0x20000500) 
[6.621] spawnCubeProgrammer(): 18:39:39:889 w ap 0 reg 16 xPSR (0x01000000) 
[6.621] spawnCubeProgrammer(): 18:39:39:889 Erasing external memory sectors [0 4]
[6.621] spawnCubeProgrammer(): 18:39:39:889 Init flashloader...
[6.621] spawnCubeProgrammer(): 18:39:39:889 halt ap 0 
[6.621] spawnCubeProgrammer(): 18:39:39:890 w ap 0 reg 0 R0 0x00000001
[6.621] spawnCubeProgrammer(): 18:39:39:890 w ap 0 reg 1 R1 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:890 w ap 0 reg 2 R2 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:890 w ap 0 reg 3 R3 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:890 w ap 0 reg 4 R4 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:891 w ap 0 reg 5 R5 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:891 w ap 0 reg 6 R6 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:891 w ap 0 reg 7 R7 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:891 w ap 0 reg 8 R8 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:891 w ap 0 reg 9 R9 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:892 w ap 0 reg 10 R10 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:892 w ap 0 reg 11 R11 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:892 w ap 0 reg 12 R12 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:892 w ap 0 reg 13 SP 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:892 w ap 0 reg 14 LR 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:892 w ap 0 reg 15 PC 0x200006C1
[6.621] spawnCubeProgrammer(): 18:39:39:893 w ap 0 reg 16 xPSR 0x01000000
[6.621] spawnCubeProgrammer(): 18:39:39:894 w ap 0 reg 17 MSP 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:894 w ap 0 reg 18 PSP 0x00000000
[6.621] spawnCubeProgrammer(): 18:39:39:894 run ap 0 
[6.621] spawnCubeProgrammer(): 18:39:39:894 halt ap 0 

 

If I do the same test for the STM32F4 processor after erase the internal FLASH memory the external loader is loaded into RAM and then the external memory is erased - lines 73...78 below.

 

[19.541] spawnCubeProgrammer(): 18:19:31:154 Memory Programming ...
[19.541] spawnCubeProgrammer(): 18:19:31:154 Opening and parsing file: ST-LINK_GDB_server_a11700.srec
[19.541] spawnCubeProgrammer(): 18:19:31:155 File : ST-LINK_GDB_server_a11700.srec
[19.541] spawnCubeProgrammer(): 18:19:31:155 Size : 30.91 KB 
[19.541] spawnCubeProgrammer(): 18:19:31:155 Address : 0x08000000 
[19.541] spawnCubeProgrammer(): 18:19:31:155 
[19.541] spawnCubeProgrammer(): 
[19.541] spawnCubeProgrammer(): 18:19:31:155 Erasing Segment <0> Address <0x08000000> Size <31612>Bytes
[19.541] spawnCubeProgrammer(): 18:19:31:155 Erasing memory corresponding to segment 0:
[19.541] spawnCubeProgrammer(): 18:19:31:156 Memory Erase via FlashLoader!
[19.541] spawnCubeProgrammer(): 18:19:31:156 Memory erase...
[19.541] spawnCubeProgrammer(): 18:19:31:159 halt ap 0 
[19.541] spawnCubeProgrammer(): 18:19:31:159 w ap 0 reg 15 PC (0x20000000) 
[19.541] spawnCubeProgrammer(): 18:19:31:159 w ap 0 reg 17 MSP (0x20000500) 
[19.541] spawnCubeProgrammer(): 18:19:31:160 w ap 0 reg 16 xPSR (0x01000000) 
[19.541] spawnCubeProgrammer(): 18:19:31:164 w ap 0 @0x20001160 : 0x00000200 bytes, Data 0x00000000...
[19.541] spawnCubeProgrammer(): 18:19:31:165 w ap 0 @0x20000000 : 0x00000004 bytes, Data 0x0000BE00...
[19.541] spawnCubeProgrammer(): 18:19:31:188 w ap 0 @0x20000004 : 0x00000D38 bytes, Data 0xF000B580...
[19.541] spawnCubeProgrammer(): 18:19:31:191 Erasing internal memory sectors [0 1]
[19.541] spawnCubeProgrammer(): 18:19:31:191 Init flashloader...
[19.541] spawnCubeProgrammer(): 18:19:31:192 halt ap 0 
[19.541] spawnCubeProgrammer(): 18:19:31:194 w ap 0 reg 0 R0 0x00000001
[19.541] spawnCubeProgrammer(): 18:19:31:195 w ap 0 reg 1 R1 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:196 w ap 0 reg 2 R2 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:197 w ap 0 reg 3 R3 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:198 w ap 0 reg 4 R4 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:199 w ap 0 reg 5 R5 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:200 w ap 0 reg 6 R6 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:201 w ap 0 reg 7 R7 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:202 w ap 0 reg 8 R8 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:203 w ap 0 reg 9 R9 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:204 w ap 0 reg 10 R10 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:205 w ap 0 reg 11 R11 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:206 w ap 0 reg 12 R12 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:207 w ap 0 reg 13 SP 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:207 w ap 0 reg 14 LR 0x20000001
[19.541] spawnCubeProgrammer(): 18:19:31:208 w ap 0 reg 15 PC 0x20000005
[19.541] spawnCubeProgrammer(): 18:19:31:208 w ap 0 reg 16 xPSR 0x01000000
[19.541] spawnCubeProgrammer(): 18:19:31:209 w ap 0 reg 17 MSP 0x20001138
[19.541] spawnCubeProgrammer(): 18:19:31:210 w ap 0 reg 18 PSP 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:210 run ap 0 
[19.541] spawnCubeProgrammer(): 18:19:31:212 halt ap 0 
[19.541] spawnCubeProgrammer(): 18:19:31:212 r ap 0 reg 0 R0 0x00000001
[19.541] spawnCubeProgrammer(): 18:19:31:212 Loader sector erase...
[19.541] spawnCubeProgrammer(): 18:19:31:214 w ap 0 reg 0 R0 0x08000000
[19.541] spawnCubeProgrammer(): 18:19:31:214 w ap 0 reg 1 R1 0x08004000
[19.541] spawnCubeProgrammer(): 18:19:31:215 w ap 0 reg 2 R2 0x00000002
[19.541] spawnCubeProgrammer(): 18:19:31:216 w ap 0 reg 3 R3 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:217 w ap 0 reg 4 R4 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:217 w ap 0 reg 5 R5 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:218 w ap 0 reg 6 R6 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:219 w ap 0 reg 7 R7 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:220 w ap 0 reg 8 R8 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:220 w ap 0 reg 9 R9 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:221 w ap 0 reg 10 R10 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:222 w ap 0 reg 11 R11 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:223 w ap 0 reg 12 R12 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:223 w ap 0 reg 13 SP 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:224 w ap 0 reg 14 LR 0x20000001
[19.541] spawnCubeProgrammer(): 18:19:31:225 w ap 0 reg 15 PC 0x2000022B
[19.541] spawnCubeProgrammer(): 18:19:31:225 w ap 0 reg 16 xPSR 0x01000000
[19.541] spawnCubeProgrammer(): 18:19:31:226 w ap 0 reg 17 MSP 0x20001138
[19.541] spawnCubeProgrammer(): 18:19:31:227 w ap 0 reg 18 PSP 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:31:227 run ap 0 
[19.541] spawnCubeProgrammer(): 18:19:31:768 halt ap 0 
[19.541] spawnCubeProgrammer(): 18:19:31:768 r ap 0 reg 0 R0 0x00000001
[19.541] spawnCubeProgrammer(): 18:19:31:768 erase: 0612ms
[19.541] spawnCubeProgrammer(): 18:19:31:768 Erasing Segment <1> Address <0x70000000> Size <37>Bytes
[19.541] spawnCubeProgrammer(): 18:19:31:769 Erasing memory corresponding to segment 1:
[19.541] spawnCubeProgrammer(): 18:19:31:769 Memory Erase via FlashLoader!
[19.541] spawnCubeProgrammer(): 18:19:31:769 Memory erase...
[19.541] spawnCubeProgrammer(): 18:19:31:771 halt ap 0 
[19.541] spawnCubeProgrammer(): 18:19:31:771 w ap 0 reg 15 PC (0x20000000) 
[19.541] spawnCubeProgrammer(): 18:19:31:772 w ap 0 reg 17 MSP (0x20000500) 
[19.541] spawnCubeProgrammer(): 18:19:31:772 w ap 0 reg 16 xPSR (0x01000000) 
[19.541] spawnCubeProgrammer(): 18:19:31:776 w ap 0 @0x20008340 : 0x00000200 bytes, Data 0x00000000...
[19.541] spawnCubeProgrammer(): 18:19:31:776 w ap 0 @0x20000000 : 0x00000004 bytes, Data 0x0000BE00...
[19.541] spawnCubeProgrammer(): 18:19:32:001 w ap 0 @0x20000004 : 0x00007F18 bytes, Data 0x00000000...
[19.541] spawnCubeProgrammer(): 18:19:32:001 Erasing external memory sectors [0 4]
[19.541] spawnCubeProgrammer(): 18:19:32:001 Init flashloader...
[19.541] spawnCubeProgrammer(): 18:19:32:002 halt ap 0 
[19.541] spawnCubeProgrammer(): 18:19:32:003 w ap 0 reg 0 R0 0x00000001
[19.541] spawnCubeProgrammer(): 18:19:32:004 w ap 0 reg 1 R1 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:005 w ap 0 reg 2 R2 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:006 w ap 0 reg 3 R3 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:007 w ap 0 reg 4 R4 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:008 w ap 0 reg 5 R5 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:008 w ap 0 reg 6 R6 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:009 w ap 0 reg 7 R7 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:009 w ap 0 reg 8 R8 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:010 w ap 0 reg 9 R9 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:012 w ap 0 reg 10 R10 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:012 w ap 0 reg 11 R11 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:012 w ap 0 reg 12 R12 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:014 w ap 0 reg 13 SP 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:014 w ap 0 reg 14 LR 0x20000001
[19.541] spawnCubeProgrammer(): 18:19:32:015 w ap 0 reg 15 PC 0x20000991
[19.541] spawnCubeProgrammer(): 18:19:32:017 w ap 0 reg 16 xPSR 0x01000000
[19.541] spawnCubeProgrammer(): 18:19:32:017 w ap 0 reg 17 MSP 0x20008318
[19.541] spawnCubeProgrammer(): 18:19:32:017 w ap 0 reg 18 PSP 0x00000000
[19.541] spawnCubeProgrammer(): 18:19:32:018 run ap 0 
[19.541] spawnCubeProgrammer(): 18:19:33:791 halt ap 0 

 

 

 

How can I fix this?

 

 

 

Tesla DeLorean
Guru
December 23, 2024

>>How can I fix this?

Remove the Internal Flash content from your External Application?

The linker script for that is evidently describing FLASH content at 0x08000000

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..