STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-L073 USB troubles.

Posted on June 08, 2017 at 09:28I am having troubles with making a USB CDC device of a Nucleo-L073.I have downloaded the STM32Cube_FW_L0_V1.9.0 projects and have tried building and running the \STM32L073Z_EVAL\Applications\USB_Device\HID_Standalone\...

Resolved! SD card no response for CMD0

Posted on May 11, 2017 at 11:09A device I had been testing for over two months suddenly started giving FR_DISK_ERR (I'm using Elm Chan's FAT-FS) [http://elm-chan.org/fsw/ff/00index_e.html]. When I tried debugging, the command (CMD0) which must be cl...

USB Audio device class on NUCLEO-F446RE

Posted on June 04, 2017 at 01:40Hi Guys,I want to experiment a bit with the USB middleware features from the CubeMX Software. My goal is to output audio from my computer via the NUCLEO board (recognized as an audio device class) and the integrated D...

i2c slave address dependency

Posted on June 05, 2017 at 00:28Hello,I want to use a STM32L100 as I2C slave with two addresses. The master will receive different size of data and different data depending on the used address. This means that the slave address also includes a comma...

nikola2 by Associate II
  • 885 Views
  • 1 replies
  • 0 kudos

STM32CubeMX 4.17.0 and USB Custom Class

Posted on October 23, 2016 at 17:45I want to configure (and program) a USB custom class (USBTMC). My question is, how do I direct the Cube Application to include the USB libraries. For now I see how to include specific classes (like HID), but not th...

sven2399 by Associate II
  • 965 Views
  • 3 replies
  • 0 kudos

STM32L4 CubeL4 bug

Posted on June 01, 2017 at 17:25I'm trying to use SPI with DMA on an L4 chip. The firmware configuration is generated by CubeMX, and it has 4 calls that check for valid DMA handles. One of these calls is:assert_param(IS_SPI_DMA_HANDLE(hspi->hdmatx))...

STM32F429 HS-USB ULPI PHY

Posted on May 30, 2017 at 13:46Please help me !!!I want to config USB STM32F429  in mode Host hight speed with USB PHY.Please tell me the way or give to me source .Thanks you so much !!!!!!#usb #stm32f429 #usb-host #stm32f4-usb-highspeed-hs-ulpi #us...