STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 USB FS and PA8 as output not working

Posted on May 17, 2017 at 15:52Hi,I'm using the STM32F446ZE.I'm using PA11 and PA12 for USB FS DM and DP, but I don't need PA8 as SOF, I need it as a simple output.USB is runing fine only if PA8 = 0 !If I set PA8 output to 1, the USB disconnects.It ...

Kuikui by Associate III
  • 4810 Views
  • 27 replies
  • 0 kudos

STM32F303VB: USB related queries

Posted on June 13, 2017 at 14:59Hi,We are using STM32F303VB on our custom hardware. We plan to use the STM32 as a USB device talking to a PC (USB Host).(I'm using STM32CubeMX (STM32Cube_FW_F3_V1.8.0) to generate project for AC6 System Workbench.)I h...

Prasant J by Associate III
  • 470 Views
  • 0 replies
  • 0 kudos

simple USB circuit

Posted on June 03, 2017 at 18:53hello,I would like to have some clarification about the USB circuit needed for the stm32f103 (and similar), I am making a simple development board just to start learning this MCUThis is taked from the maple mini https...

0690X00000607DzQAI.png

Writing a custom USB CCID device class

Posted on June 08, 2017 at 10:21Hi Everyone!I am starting to work on a new project, and I want to select a microcontroller platform. I love stm32, so I'm hoping there is a way around what I think will be a problem.I have searched in ST forums and on...