User Activity

Posted on August 04, 2017 at 08:06Hello,I have troubles with the STM32L467. I am using the RTC without any extra settings like alarm or tamper. I have set the time via STM32Cube and at some points in the code the chip reads out the time.My problem i...
Posted on June 05, 2017 at 00:28Hello,I want to use a STM32L100 as I2C slave with two addresses. The master will receive different size of data and different data depending on the used address. This means that the slave address also includes a comma...