STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L432KC Internal bootloader issue

I am trying to access the STM32L432KC internal bootloader through BOOT0(PH3) pin. Option bytes are set as - 0x0FFFF8AAie.nSWBOOT0 = 1nBOOT1 = 1BOR_LEV  = 000RDP(Read protection level) = 0xAA (read protection inactive)This is how option byte...

Resolved! Why does a timer operating in interrupt mode generate an update event immediately after intialization?

HelloI have TIM3 set up like so:ABP1 Timer clock = 84 MHzPrescaler = 8399Period 9999Update event selected as triggerNVIC enabled for TIM3 global interruptThis gives me a timer interrupt every 1 second. But it appears as though the callback HAL_TIM_Pe...

Always getting SPI OVR Error instead of executing SPI RX callback functions while interfacing SPI1 + DMA + STM32H7

For DMA, allocating the buffer to the right memory segment,I am already allocating the buffer in to D2 (0x30000000), which I think should be right, and I haven't enabled the cache yet, for remaining all nonvolatile memory allocated in section D1 (0x2...

0690X0000087ZcfQAE.png 0690X0000087ZckQAE.png 0690X0000087ZczQAE.png 0690X0000087Zd4QAE.png

STM32F7 IAP using DFU & USB MSC

Hi all, On an STM32F746-Disco I've succesfully tested DFU using DfuSe demo (ie sending a .dfu file from a PC to the board using the USB as a serial port) and the USB Host MSC... I wonder if it's possible create a bootloader that will read a dfu fil...

iw2lsi by Associate III
  • 2210 Views
  • 2 replies
  • 0 kudos