User Activity

Hi.We are trying to configure lsm6dsl to catch peak shock. The usecase is that the sensor should sleep until shock occurs (say above 1g on any axis), cause interrupt and have the value available in FIFO. We are using the STMems_Standard_C_drivers fro...
Posted on October 16, 2017 at 14:38Hi.I'm trying to output 24khz mono pcm data over SAI to wm8994 codec. 16khz mono seems to work OK, but 24 is not supported by ST by default. I've made some changes for the support to codec and sai init. Now I wonde...
Posted on September 11, 2017 at 14:50Hi.I'm using the SSL_client example as base for my project. I've incorporated parts from FMC_SDRAM example as I need to use the largish buffers for audio stuff.However as I didn't seem to be able to get IP anymor...
Posted on August 30, 2017 at 09:33Hi.So both mbed tls examples in F7 v.1.7.0 seem to fail to compile. Few others I've tried from same SDK seem to compile & work ok.First issue seems to be the preprocessor parameter for mbedtls_config.h. I couldn't s...
Posted on June 27, 2017 at 15:02Hi.I'm trying to use DMA to  drive PWM output for led effects. MCU write seems to be OK, however there's few very weird consepts related to DMA configuration I don't seem to be able to wrap my head around.void HAL_TIM...
Kudos from