STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32u5 ADC is not reading using DMA

Split from this thread. (new question) You might be right. However it was made based on the well described example I have found. https://deepbluembedded.com/stm32-adc-multi-channel-scan-dma-poll-single-conversion/ I was trying tu run DMA but it was n...

aristot by Associate II
  • 1328 Views
  • 6 replies
  • 0 kudos

Resolved! CMSIS version

The STM32CubeG4 package comes with CMSIS v5.6 (https://github.com/STMicroelectronics/STM32CubeG4/tree/master/Drivers/CMSIS) which I think was released in July 2019.Is it necessary to use this version or can I upgrade it to a later release? Currently ...

Repwoc by Associate III
  • 3690 Views
  • 11 replies
  • 3 kudos

Unable to listen with UDP socket in STM32F756ZG

Hi all,          I'm using the STM32F746ZG Nucleo (CubeF7 LwIP HTTP Server Netconn RTOS example). I start my app when the netif gets a valid IPv4 using netif_set_status_callback (LWIP_NETIF_STATUS_CALLBACK=1) and then bind a UDP socket on the assigne...

VasuV by Associate II
  • 396 Views
  • 0 replies
  • 0 kudos

Resolved! STM32U585 SDcard read and write using FILEX

Hello everyone,I am working with an ST M 32 U 585 V I T micro controller and I would like to use an SD card for file read/write operations using Azure File X.I have enabled Thread x and File X middle ware in S T M 32 Cube IDE (Cube M X), but I am not...

yugi by Associate II
  • 579 Views
  • 2 replies
  • 0 kudos

Resolved! Jump from Openbootloader to the Application

Greetings! So, I used the OpenBootloader project, and then flashed a GPIO_IOToggle firmware in other area of the flash, close to the example in the video Introduction to Open Bootloader, Part 3: Loading an Application.  In that example the CubeProgra...

Resolved! USB microphone example with USBX

Hi,Could you please let me know if you’re planning to provide an example of a USB Audio device based on USBX in the near future?By the way, the ST X-CUBE-AUDIO package is based on TinyUSB that is not officially supported. I’m wondering whether it’s f...

ERROR by Senior
  • 645 Views
  • 2 replies
  • 2 kudos