STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Developing/Integrating AWS and MQTT Stacks

I have integrated lwip on my STM32H563RGT6  library and my requirement is to establish connection to my AWS endpoint from MCU to the cloud along with certificates. help me by providing the necessary stacks.Were my requirement is to send/publish some ...

aravindpv by Associate III
  • 530 Views
  • 1 replies
  • 1 kudos

USB HID Stm32f767

Hello, I've built a project with an STM32F767 and a USB HID connection. I also have a Visual Studio 2010 application to set PA0 to 1 for testing. My connection is established, and in Device Manager, the USB Custom HID device is recognized, but I can'...

PSEBA.1 by Associate II
  • 472 Views
  • 1 replies
  • 1 kudos

Resolved! Using USB-PD SRC and USB-CDC Device together

Hi @FBL I am working on a similar project like This one (USB CDC ACM device with Power Delivery in Source mode using USBX in standalone mode, FreeRTOS and USBPD with a TCPP02). The STM32 used is the H573I.I have found some code to add in the function...

Aristy by Associate II
  • 1042 Views
  • 7 replies
  • 1 kudos

One Pulse Mode not working

My goal is to use timers to follow the required timing steps for a module I’m working with. To achieve this, I decided to use two timers — TIM1 and TIM2.TIM2 is responsible for counting the T1 time step. For this, I’m using One-Pulse Mode, so TIM2 is...

MichalPorazko_0-1762109266115.png MichalPorazko_2-1762110115913.png MichalPorazko_3-1762110191312.png

Resolved! Using ThreadX Version 6.1

Hi All, I am using ThreadX on an STM32H753. The version of ThreadX being used is 6.1. I use this older version because it is ISO-62304 certified. All is functioning as desired but each time I execute code generation from CubeMX the ThreadX files are ...

Gil1 by Associate III
  • 691 Views
  • 4 replies
  • 0 kudos

STM32F407 connected to KSZ8863 switch

I have read these forums and I see some have successfully got the F407 connected to KSZ8863 working. I am trying to do a simple non managed switch RMII PHY connection to the third port with no luck. I have confirmed the 50mhz clock input to the KSZ88...

bradbas by Associate II
  • 555 Views
  • 0 replies
  • 0 kudos

Stm32l011 refuses to go into stop mode

Hello everyone, I have a problem with my STM32L011G4U6, I want to put it in stop mode or in standby mode, but the two modes are not taken into account, only the sleep mode works, I must surely make a mistake but where? here is my function:   void E...