STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H743_EVAL USB_HOST/HID_Standalone example.

The main loop of the HID_Standalone example is: while(1) { USBH_Process(&USBHost); HID_MenuProcess(); } The problem is when a slow process is put in the loop: while(1) { HAL_Delay(10); //or any slow process > 8ms USBH_Process(&USBHost)...

Asantos by Senior
  • 610 Views
  • 1 replies
  • 1 kudos

STMF0 I2C Slave IT states

I have a STM32F030C6 on a custom board and I want to use it as an I2C slave device.With the example given with the cube hal (FW 1.9) I got it working. Kind of.I can write data from the master to the slave. But I have problems reading data from the de...

0690X0000089c3mQAA.png 0690X0000089c3rQAA.png
BNeum by Associate II
  • 894 Views
  • 1 replies
  • 0 kudos

Resolved! Pack IAP and application in same binary

Hi, Want to be able to flash the target device( an STM32F446) using a propritary CAN interface. EI not use the bootloader default CAN flashing method. As i understand it I must first make a IAP binary and flash using the bootloader by SWD. To then ad...