STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB DFU on STM32L496

Hello,I am trying to enable USB DFU functionality on a custom board with STM32L496 MCU.Only D+ and D- pins are routed from the USB connector to the MCU, ID is not routed at all and VBUS is only to power the board. I added a code in my firmware that j...

EKirs by Associate II
  • 658 Views
  • 0 replies
  • 0 kudos

STM32f722 USB_OTG_HS doesn't work in FS mode

Trying to connect two FS devices to an STM32F722RET. Datasheets are a little vague, but seems it should be OK as long as I don't do HS.Using cubeMX, and for the FS port (PA11/PA12) - things work great. For the HS port (configured to be host_only, F...

InvZim by Associate
  • 407 Views
  • 0 replies
  • 1 kudos

Resolved! Is there I2C Bootloader on STM32L051K8?

I am using STM32L051K8 MCU in my project. All the project has been developed. Now there is a need to provide OTA firmware upload. For that I require to use I2C bootloader as I have alreadey interfaced I2C EEPROM. Please let me know whether it is poss...

AJadh.5 by Associate
  • 1025 Views
  • 3 replies
  • 0 kudos