cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f722 USB_OTG_HS doesn't work in FS mode

InvZim
Associate

Trying to connect two FS devices to an STM32F722RET. Datasheets are a little vague, but seems it should be OK as long as I don't do HS.

Using cubeMX, and for the FS port (PA11/PA12) - things work great. For the HS port (configured to be host_only, FS 12mbit) - I'm getting nothing.

Traced things back to OTG_HS_IRQHandler, which never fires, so phost->gState stays in HOST_IDLE.

Not sure where to take it from here..

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0