STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Push Pull PWM

Hello ST, I am having some trouble generating two PWM signals for a push pull converter.  Ideally I would like the PWM outputs to look like this, I would like the PWM frequency to be 100kHz and a duty cycle range of 0% to 50%. I have connected the p...

allanoverst_0-1762377988597.png PWM PA0 and PA1.png

Resolved! USB PD Source Capabilities send too early

Hi ST Community,once again I have found a USB PD Specification violation, that I can't find the reason for:Source operation: According to USB PD Spec the order of action is as follows:1. Detect Sink using CC lines and only if sink is detected continu...

abtq by Associate III
  • 2476 Views
  • 9 replies
  • 4 kudos

Resolved! STM32H503 I2C communication speed on I3C bus.

Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code. Hello! I connect one I2C target and one I3C target device...

GH502_0-1762333926524.png
GH502 by Associate II
  • 926 Views
  • 5 replies
  • 1 kudos