STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART3 overrun interrupt

Hello,It is the first time I am using STM32 and migrating my code from texas instruments controller using USART3. I want to receive data and then transmit data of different sizes. I get a problem that I see appears often but in my case I cannot see w...

GTanova by Associate III
  • 2120 Views
  • 15 replies
  • 13 kudos

Ethernet Request time out issue

  Hello everyone, I am working with an STM32H5 series board and have successfully initialized Ethernet using the lwIP stack.The DHCP process works correctly — I am able to obtain an IP address. However, I am facing a “Request Timeout” issue when I tr...

Resolved! UART output is garbled on Tera Term

I ran the example project and successfully displayed “Hello World” on Tera Term.Then I tried to port this project into my own one.However, the result was garbled characters in the terminal.The baud rate (115200) and PLL/clock configuration are the sa...

chachamaru_0-1762764753839.png chachamaru_1-1762764754652.png chachamaru_2-1762764753839.png chachamaru_3-1762764753837.png

USB microphone from the USB speaker example

Hi,Tried to convert STM32CubeN6\Projects\STM32N6570-DK\Applications\USBX\Ux_Device_Audio_2.0 example of the USB speaker to the USB microphone on STM32N6570-DK.The USB device is enumerated as an audio recording device, ux_device_class_audio_stream_fra...

ERROR by Senior
  • 447 Views
  • 1 replies
  • 0 kudos