STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f3 STD lib ADC init problem

Hello everyone.I have problem with ADC module of STM32F3. I have two board, one board use STM32F334K8T6 is the first version of my prototype, one board use STM32F334C8T6 is new version. I have use ADC module in my program and using STD lib. but with ...

thang le by Associate
  • 1116 Views
  • 1 replies
  • 1 kudos

Troubles with FreeRTOS-HardFaults-Mallocs etc

Hello all,i'm facing a lot of troubles to run my server application on stm32.The server runs in a task. I'm using FreeRTOS. I can't explain everything here but i can share the code.First of all my application goes into HardFault in a kinda random way...

AGaru by Associate III
  • 3483 Views
  • 7 replies
  • 0 kudos

STM32H743xx Version V Bootloader init issue !!

Hi All,I have a strange problem entering the Bootloader.I need to send 0x7F twice to enter Bootloader. Details: I am working on a project where I need to program STM32H743xx MCU via UART pins. I was successful in programming STM32H743xx “Version Y�? ...

James1 by Associate II
  • 2235 Views
  • 4 replies
  • 0 kudos

X_cube AWs OTA isn't working

I am using p-l496G-cell1 with x-cube-AWSThe communication between AWS and P-l496-CELL01 via MQTT is work fine But OTA update is not working.I follow steps according to manual• Store the .sfb firmware file on AWS S3 service (in an S3 bucket; for examp...

pragnesh by Associate III
  • 1007 Views
  • 1 replies
  • 0 kudos

Why DAC make 0.12[V] when I set it be 0

HAL_DAC_Start_DMA(&hdac, DAC_CHANNEL_1, (uint32_t*)setdac, 1, DAC_ALIGN_12B_R);HAL_DAC_SetValue(&hdac, DAC_CHANNEL_1, DAC_ALIGN_12B_R, setdacvalue);The first problem was when I changed setdac which points value that DMA buffer(?) It doesn't work so I...

0690X00000BvbglQAB.png
SKim.1761 by Associate III
  • 1822 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G0 project created by CubeMX does not work

The hardware I have is the STM32G0 Discovery Kit. The sample code using this hardware works normally. I tried to rebuild a project using CubeMX. I found that it would be in CHECK_PE_FUNCTION_CALL (USBPD_PE_Init (USBPD_PORT_0, (USBPD_SettingsTypeDef *...

Yqiwu.1 by Associate
  • 1575 Views
  • 2 replies
  • 0 kudos