STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 USB-HOST (dis)connect bouncing

Hi all,I have a STM32H743 running at 400MHz with simple USB 1 wiring to an USB A jack. It works fine, no issues, runs for hours with thousands of read and write operations.But there is one little issue that drives me crazy:If I plug in and unplug one...

Microman by Associate III
  • 6300 Views
  • 10 replies
  • 1 kudos

FDCAN Tx Interrupts

Hi, I'm trying to configure STM32H7 and STM32G4 FDCANs to generate an ISR on transmit complete frame.I call the functios to enable respective ISRs:HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_TX_COMPLETE, 0);  HAL_FDCAN_ActivateNotification(&hfd...

Asantos by Senior
  • 5338 Views
  • 3 replies
  • 2 kudos

stm32f3xx__ll__comp.h bug

Hello,This line in the mentioned library is faulty.#define LL_COMP_OUTPUT_TIM3_IC1_COMP2 (COMP_CSR_COMPxOUTSEL_3 | COMP_CSR_COMPxOUTSEL_1 | COMP_CSR_COMPxOUTSEL_0) /*!< COMP output connected to TIM3 input capture 1 (specific to COMP instance: COMP...

STM32F411E-DISCO CubeMX's repository issue

Hello, I've find one hidden fail in template project for STM32F411E-DISCO (STM32Cube\Repository\STM32Cube_FW_F4_V1.24.1\Projects\STM32F411E-Discovery\Templates). In header file inc/stm32f4xx_hal_conf.h there is a wrong define of hse frequency:#if !de...

AMoro.16 by Associate II
  • 1045 Views
  • 1 replies
  • 0 kudos

I am implementing a ZERO COPY COPY driver for the STM32H7 eth module using PHY DP83825i. Something is strange, the communication stop every 9 seconds for 1 to 2 seconds. but it seem to be at the low level (hardware).

 Even on the Iperf client, there is a dip in transmission bandwidth and we can see the router lights, they all goes off with few ARP request. We are using FreeRTOS+TCP. we have another module using LWIP on other PHY + CPU combination and working with...

ARoye.1 by Associate
  • 1857 Views
  • 2 replies
  • 0 kudos

Can I have DFU and CDC printf on the same usb port?

I want to do both firmware updating via dfu and have serial data output on the STM32G431KB without having to press any boot switch or changing usb ports.In my code I can probably jump to the bootloader, without having to pull high boot0 pin.But can I...

WSpar.1 by Associate III
  • 2366 Views
  • 8 replies
  • 0 kudos