STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet frame length issue

Hi, I got a problem when I use the Ethernet TCP stack and hope someone can help me figure it out.I am using tcpecho protocol to communicate between PC and the board. PC send the command and board response with the data. If I just send 64 bytes, as: ...

kqian by Associate II
  • 2910 Views
  • 5 replies
  • 0 kudos

STM32F746 Discovery board USB MSC example

hello,we would like to run USB MSC example using STM32CUbe IDE toolsSTM32IDE V1.3HAL V1.16hardware STM32F746 Discovery boardUsing Internal USB PHY, 12 Mbit.we start with demo applications located \\STM32Cube\Repository\STM32Cube_FW_F7_V1.16....

IB.1 by Associate III
  • 1078 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H7 nucleo USB FS CDC

Posted on November 09, 2017 at 10:37Hi,I am trying to start with USB CDC on stm32h7. I create new project with CubeMx + STM32Cube_FW_H7_V1.1.0 (cubemx file attached). After compile usb device doesnt appear on the system.RegardsMike#stm32h743 #virtua...

embvis by Associate III
  • 12475 Views
  • 19 replies
  • 1 kudos