STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 USB Host Library - HID Class Issues

Im trying to connect a keyboard to a STM32F407 discovery board.The board correctly identifies the keyboard and works as expected, for the most part, except I cant get the multimedia keys and the "regular" keys to work at the same time. The keyboard i...

PMera.1 by Associate III
  • 1714 Views
  • 3 replies
  • 0 kudos

Sending float voltage value via USB CDC.

Hello,I want to send the float type voltage value that I read with stm32f429I discovery card using adc reference voltage via usb cdc. My problem is this; I read the adc reference voltage and voltage value, and I can assign it to a float type variable...

BTaşk.1 by Associate II
  • 3152 Views
  • 4 replies
  • 0 kudos

DFU file manager

Good morning,I'm working with STM32L4 and I have created my own bootloader.In order to program the MCU, I use USB interface, so I need the DFU file. I use the 'DFU File Manager' tool to create the DFU file from the HEX file. It works fine, but then, ...