STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to get peripheral clock programmatically?

Hello,I have a generic function for the timer configuration. The time base address is an input parameter to this function. I'm looking for a way to get the timer clock so that I can set the timer prescaler. How can I do that with HAL?I guess I need t...

GregB by Associate II
  • 2640 Views
  • 3 replies
  • 0 kudos

Boot app code from external memory OSPI/QSPI ???

Hello!I'am playing with the STM32H7B3-DK and I have successfully bring up the board and run a custom gui:The GUI assets are loaded in the external OSPI and the dual framebuffer is placed in the the external SDRAM.Now I'am interested in loading also t...

PLago.2 by Associate II
  • 1819 Views
  • 3 replies
  • 0 kudos

Code not working after relocate my vector table.

Hi,STM32f429ii. FreeRtos.I have relocated my vector table from default address into 0x8008000 since my bootloader firmware is placed on in the default start address (0x8000000). I am using IAR workbench, i have modified the vector table address as 0x...

I2C bootloader for STM32Lxx

Hello, I've been looking at two MCUs in particular (STM32L010C6 and STM32L100C6). According to the AN2606 application note, they should support I2C flashing, but the product page only mentions USART and SPI. Which one is the correct answer?Thanks!

NTzov.1 by Associate
  • 1196 Views
  • 1 replies
  • 0 kudos