cancel
Showing results for 
Search instead for 
Did you mean: 

MSC USB not working with TCP stack

kqian
Associate II

Hello,

I am working on the customized board with MCU STM32F767 + + LAN8742A + freeRTOS. The USB MSC host was working if no TCP server code was added. But when I add the TCP code, MSC is not working any more.

The code is as below:

if tcpip_init(NULL, NULL); is commented, USB host can work, I can write file to the USB MSC. but if uncommented, the code never run to the HOST_USER_CLASS_ACTIVE and disk cannot mounted in the USBH_UserProcess2(). So far I can see the function static USBH_StatusTypeDef USBH_MSC_Process(USBH_HandleTypeDef *phost) is not called. Is it caused by the freertos? anyone has similar issue and how to solve it?

Thanks

static void StartDefaultTask(void const * argument)

{

MX_GPIO_Init();

// tcpip_init(NULL, NULL);

// Netif_Config();

// tcpecho_init();

 osThreadDef(MSC_Thread, MSCTask, osPriorityHigh, 0, 1 * configMINIMAL_STACK_SIZE);

osThreadCreate(osThread(MSC_Thread), NULL);

 for(;;)

 {}

}

/**

 * @brief USBH_UserProcess2

 * @param phost: MSC Host handle

 * @param id:  MSC Host Library user message ID

 * @retval None

 */

static void USBH_UserProcess2 (USBH_HandleTypeDef *phost, uint8_t id)

{

 /* USER CODE BEGIN CALL_BACK_21 */

 switch(id)

 {

 case HOST_USER_SELECT_CONFIGURATION:

 break;

 case HOST_USER_DISCONNECTION:

osMessagePut(AppliEvent, MSC_APPLICATION_DISCONNECT, 0);

  if (FATFS_UnLinkDriver(USBDISKPath) == 0)

  {

  }

  break;

 break;

 case HOST_USER_CONNECTION:

osMessagePut(AppliEvent, MSC_APPLICATION_READY, 0);

 break;

 case HOST_USER_CLASS_ACTIVE: 

//Appli_state_MSC = MSC_APPLICATION_READY;

osMessagePut(AppliEvent, MSC_APPLICATION_READY, 0);

  if (FATFS_LinkDriver(&USBH_Driver, USBDISKPath) == 0)

  {

   if (f_mount(&USBH_fatfs, "", 0) != FR_OK)

   {

//    LCD_ErrLog("ERROR : Cannot Initialize FatFs! \n");

   }

else

{

MSC_Connected =1;

}

  }

 break;

 default:

 break;

 }

 /* USER CODE END CALL_BACK_21 */

}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
kqian
Associate II

I tried to do the similar thing on STm32F746 discovery board but not successes. I cannot find the TCP echo code with the LAN8742A ethernet chip. Does it mean I have to use DP83848 ethernet chip to get the TCP echo server function?

Thanks

kqian
Associate II

Sorry, I am talking the TCP echo server with FreeRTOS.