STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo-f446re internal dac

    /* USER CODE BEGIN Header */ /** ******************************************************************************* * @file : main.c * @brief : Main program body ************************************************************...

harry123 by Senior II
  • 8540 Views
  • 24 replies
  • 15 kudos

CAD Model for STM32H743 EVAL kit

Hi, Currently using a STM32H743X Eval kit ...it has the 6" screen on it.  I've check in the CAD files for the EVAL kit but its got the gerbers BOM ect.. but no complete CAD ... as in something we can import into solidworks , so were able to model bit...

Brushless motor driver

Hello, I have a Brushless motor driver PCBA quantity of 70 such drivers and according to their original designThere are 3 units of THT Electrolytic capacitor 100V 220uf on itAnd it has 6 units of Power Mosfet 100V 107ABecause it is 100V, it can be us...