Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Posted on May 14, 2014 at 17:57I have both an STM32 Nucleo and STM32F429I-DISCO discovery board. On the Nucleo the ST-LINK is version 2-1 which creates a virtual COM port on Windows that is connected to USART1 of the target MCU. This is very handy f...
Posted on November 06, 2015 at 06:41I'm using Keil uvision(on windows 7 as well as windows 8.1) to implement ADC & DAC functions on STM32F4-Discovery board. After my last trial, ''ST-Link Connection Error'' occurred and ever since, I need to do a ''...
Posted on October 06, 2015 at 13:32Hello all,I'm using two Nucleo-F401RE boards which do some cross communication and timing monitoring. Initally I used boards with revision C-01 and HSI as clock source. This worked fine when doing individual clock-...
Posted on October 17, 2015 at 18:49Hi Community, I was using a NetDuino 2 Board which is just an STM32F205. Since I couldn't get the USB HID device to work correctly I thought I would take a shot at making my own firmware for the board. I created a ...
Posted on October 06, 2015 at 06:12I have a new STM32F401 discovery board, but the on-board ST-LINK stops responding only after a few programming. It shows ''internal command error''. I have to press the reset button when I want to program/debug the...
Posted on September 21, 2015 at 10:45Is the ST-Link/V2 able to supply power to the target?The UM1075 User Manual is not at all clear on this.AIUI, 'VAPP' (pins 1 & 2 on the 20-pin JTAG/SWD connector) provides the supply voltage from the target; ie, ...
Posted on September 16, 2015 at 00:04Hi.I have just upgraded one of our boards from using the STM32F030C8T6 to the more or less pin-compatible STM32F030CCT6.The only change that had to be made was to supply the one extra power supply rail to pin 35 ...
Posted on October 06, 2011 at 00:58Is there any possibility of Mac or Linux drivers for programming the STM32L board. I intend to use this for a class next year (Jan 2012) to introduce micro controllers and I wanted the students to bring the board h...
Posted on September 10, 2015 at 16:53I'm looking for a good source of either developed external loaders for the ST-Link V2 or a good reference on modifying the existing loaders that come with the ST-Link utility, I am trying to program a NOR flash (...
Posted on August 23, 2015 at 14:55Hello,First of all i am new to all of this programming.I am using a St-Link/V2 Isol but everytime i want to connect to the target i get this messageCan not connect to target!Please select ''Connect Under Reset'' mod...